Evaluation board for BLDC motor control using FOC

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
cw2611
Level 3
Level 3
25 sign-ins 25 replies posted 10 questions asked

Hey!

I want to run a 36 V BLDC motor with peak current at 11 A. Do you have any evaluation board that contains both the microcontroller as well as the half bridge? I want to implement FOC.

0 Likes
1 Solution
psb
Moderator
Moderator
Moderator
250 sign-ins 25 solutions authored 100 replies posted

Hello @cw2611 ,

   Currently, we do not have a complete solution ( controller + inverter (and) PFC ) for driving the BLDC motor with the above mentioned specifications. 
However, the following are the evaluation boards other than/along with the already mentioned boards in the thread which can be added to aid your design. 

  1.  kit_xmc4400_dc_v1 
  2. kit_xmc1300_dc_v1 
  3. kit_xmc750watt_mc_ak_v1 
  4. eval_tolt_dc48v_3kw 
  5. kit_xmc13_boot_001 
  6. kit_xmc14_boot_001 
Best Regards,
Sai

View solution in original post

0 Likes
4 Replies
psb
Moderator
Moderator
Moderator
250 sign-ins 25 solutions authored 100 replies posted

Hello @cw2611 , 

Can you please let us know the following information, along with the XMC controller you might want to prefer : 
1. DC Bus Voltage Range
2. Maximum continuous output current (at lowest inout voltage, max torque, etc)
3. Starting current
4. Application for which you need the design.

We have KIT_MOTOR_DC_250W_24V to suggest for now, which can use the XMC cards KIT_XMC1300_DC_V1KIT_XMC1400_DC_V1KIT_XMC4400_DC_V1.

Kindly let us know the details and also if these boards work out for you. 

Best Regards,
Sai
0 Likes
User12789
Level 3
Level 3
10 sign-ins First solution authored 5 sign-ins

The "Kit Motor DC 250W" board won't support your 36V 11A motor at full output. As the name says, it's a 250W board. This board will work if you keep the current below the board's limit.

I don't believe Infineon has a motor control board in between their 250W and 750W boards. The 750W board probably isn't a good fit for your application since the minimum Vdc it supports is over 100V.

0 Likes
cw2611
Level 3
Level 3
25 sign-ins 25 replies posted 10 questions asked

1. DC Bus Voltage Range: 36V to 50V
2. Maximum continuous output current: 8A

0 Likes
psb
Moderator
Moderator
Moderator
250 sign-ins 25 solutions authored 100 replies posted

Hello @cw2611 ,

   Currently, we do not have a complete solution ( controller + inverter (and) PFC ) for driving the BLDC motor with the above mentioned specifications. 
However, the following are the evaluation boards other than/along with the already mentioned boards in the thread which can be added to aid your design. 

  1.  kit_xmc4400_dc_v1 
  2. kit_xmc1300_dc_v1 
  3. kit_xmc750watt_mc_ak_v1 
  4. eval_tolt_dc48v_3kw 
  5. kit_xmc13_boot_001 
  6. kit_xmc14_boot_001 
Best Regards,
Sai
0 Likes