Not applicable
Aug 04, 2017
04:01 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 04, 2017
04:01 AM
Hi All,
I have XMC1300 kit and pin P2.5 potentionmeter is connected as it is analog pin also.
I want to use this pin as key input digital pin on my application design. But before that I tried to work on XMC1300 kit.
My aim is to use falling edge on this pin P2.5 through ERU to generate an interrupt.
Based on the example below
But issues I am getting are:
As P2.5 is analog pin I had made it Input pin for key. Some where I read that Analog Pin for making digital input I have to use XMC_GPIO_EnableDigitalInput(XMC_GPIO_PORT2, 5); so I have used this also.
But still I am not getting the correct result.
Please guide me where I am doing wrong.
Regards,
Tinchu
I have XMC1300 kit and pin P2.5 potentionmeter is connected as it is analog pin also.
I want to use this pin as key input digital pin on my application design. But before that I tried to work on XMC1300 kit.
My aim is to use falling edge on this pin P2.5 through ERU to generate an interrupt.
Based on the example below
XMC_ERU_ETL_CONFIG_t button_event_generator_config =
{
.input = ERU0_ETL1_INPUTA_P2_5,
.source = XMC_ERU_ETL_SOURCE_A,
.edge_detection = XMC_ERU_ETL_EDGE_DETECTION_FALLING,
.status_flag_mode = XMC_ERU_ETL_STATUS_FLAG_MODE_SWCTRL,
.enable_output_trigger = true,
.output_trigger_channel = XMC_ERU_ETL_OUTPUT_TRIGGER_CHANNEL0
};
XMC_ERU_OGU_CONFIG_t button_event_detection_config =
{
.enable_pattern_detection = false,
.service_request = XMC_ERU_OGU_SERVICE_REQUEST_ON_TRIGGER
};
XMC_ERU_ETL_Init(ERU0_ETL1, &button_event_generator_config);
XMC_ERU_OGU_Init(ERU0_OGU0, &button_event_detection_config);
NVIC_SetPriority(ERU0_0_IRQn, 15);
NVIC_ClearPendingIRQ(ERU0_0_IRQn);
NVIC_EnableIRQ(ERU0_0_IRQn ) ;
void ERU0_0_IRQHandler(void)
{
XMC_ERU_ETL_ClearStatusFlag(ERU0_ETL1);
}
But issues I am getting are:
- Continuous interrupt is generating irrespective of P2.5 voltage level(digital high or low)
- If I try to use any interrupt other than ERU0_0_IRQHandler, its not working
As P2.5 is analog pin I had made it Input pin for key. Some where I read that Analog Pin for making digital input I have to use XMC_GPIO_EnableDigitalInput(XMC_GPIO_PORT2, 5); so I have used this also.
But still I am not getting the correct result.
Please guide me where I am doing wrong.
Regards,
Tinchu
- Tags:
- IFX
0 Replies