Not applicable
Feb 03, 2016
12:08 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 03, 2016
12:08 AM
Hi All,
setup : xmc1300 kit + DAVE 4.
I have two digital inputs connected to the ERU unit and then performing an logical AND. This signal I want to use for the TRAP signal into the CCU8. Everything compiles, without errors nor warnings, but the TRAP functionality obviously does not work as it should.
I have attached code showing the XMC failure to combine the ERU with TRAP functionality.
Code overview:
- DIO_PWM1_H0, P2.4 -> Connects to ED_PWM1_H, signal a
- DIO_PWM1_H1, P2.2 -> Connects to ED_PWM1_H, signal b
- DIO_PWM1_T1, P2.5 -> Connects to ED_TRAP, signal a
- DIO_PWM1_T2, P2.1 -> Connects to ED_TRAP, signal b
- PWM_CCU8_0, P0.0
* ED_PWM1_H (logical AND)- starts the PWM on event0 - This works
* ED_TRAP (logical AND) - should perform trap on event2 - This just fails
If anyone can comment on the ERU unit and the TRAP functionality that would be useful. For now it seems that there is a bug somewhere in the hardware.
Regards
Enigma
setup : xmc1300 kit + DAVE 4.
I have two digital inputs connected to the ERU unit and then performing an logical AND. This signal I want to use for the TRAP signal into the CCU8. Everything compiles, without errors nor warnings, but the TRAP functionality obviously does not work as it should.
I have attached code showing the XMC failure to combine the ERU with TRAP functionality.
Code overview:
- DIO_PWM1_H0, P2.4 -> Connects to ED_PWM1_H, signal a
- DIO_PWM1_H1, P2.2 -> Connects to ED_PWM1_H, signal b
- DIO_PWM1_T1, P2.5 -> Connects to ED_TRAP, signal a
- DIO_PWM1_T2, P2.1 -> Connects to ED_TRAP, signal b
- PWM_CCU8_0, P0.0
* ED_PWM1_H (logical AND)- starts the PWM on event0 - This works
* ED_TRAP (logical AND) - should perform trap on event2 - This just fails
If anyone can comment on the ERU unit and the TRAP functionality that would be useful. For now it seems that there is a bug somewhere in the hardware.
Regards
Enigma
2 Replies
Not applicable
Feb 03, 2016
12:37 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 03, 2016
12:37 AM
Hi All,
Here is an even simpler example of not being able to use the ERU and TRAP together.
Same setup as before.
Code (see attached):
- DIO_IN - P 2.4, connected to the event detector
- DIO_OUT - P0.0, the OGU pdout is connected to this pin
Idea : P0.0 should have the same signal as on P2.4. (Simple test)
Result : The ERU fails to produce the correct trap signal.
Regards
Enigma
Here is an even simpler example of not being able to use the ERU and TRAP together.
Same setup as before.
Code (see attached):
- DIO_IN - P 2.4, connected to the event detector
- DIO_OUT - P0.0, the OGU pdout is connected to this pin
Idea : P0.0 should have the same signal as on P2.4. (Simple test)
Result : The ERU fails to produce the correct trap signal.
Regards
Enigma
Feb 16, 2016
09:15 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 16, 2016
09:15 AM