Jun 09, 2019
04:49 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 09, 2019
04:49 AM
Hallo Everyone!
Attached a sample project where I have the VADC and DMA running together using the DAVE 4.4.2 CE apps
I am using 2X VADC groups, each with 3 inputs, sampling in continuous mode
With 2X DMA channels running (one for each VADC group), transferring the result registers to RAM
DMA transfers are triggered on the VADC result ready event.
I hope this is of help to someone out there.
Instructions to build are all at the start of main.c please follow it to regenerate source files as I had to delete all the generated files to save space
Ive had to split the zip file into 2 files to stay below the 10MB limit, unzip them into the same directory
Kind regards
Gert van Biljon
Attached a sample project where I have the VADC and DMA running together using the DAVE 4.4.2 CE apps
I am using 2X VADC groups, each with 3 inputs, sampling in continuous mode
With 2X DMA channels running (one for each VADC group), transferring the result registers to RAM
DMA transfers are triggered on the VADC result ready event.
I hope this is of help to someone out there.
Instructions to build are all at the start of main.c please follow it to regenerate source files as I had to delete all the generated files to save space
Ive had to split the zip file into 2 files to stay below the 10MB limit, unzip them into the same directory
Kind regards
Gert van Biljon
0 Replies