Mar 08, 2019
02:54 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 08, 2019
02:54 AM
Hello,
When I installed the 'Infineon-Memtool-DT-v04_77-EN' memtool from Infineon, I got an error when it started installing the DAS part.
I got the following error: 'Unable to create file'. I was running the setup as an administrator.
Manually installing v6 or v7 of the DAS files gave same error.
I'm using Windows 10/64bit operating system.
Someone an idea?
Thanks.
Wim
When I installed the 'Infineon-Memtool-DT-v04_77-EN' memtool from Infineon, I got an error when it started installing the DAS part.
I got the following error: 'Unable to create file'. I was running the setup as an administrator.
Manually installing v6 or v7 of the DAS files gave same error.
I'm using Windows 10/64bit operating system.
Someone an idea?
Thanks.
Wim
- Tags:
- IFX
0 Replies
This widget could not be displayed.