Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
hgoo
Level 1
Level 1
First question asked Welcome!

I am now using EVBD-XMC4200 platform2go for Arduino. When I waw deBugging, I had the following console.

----------------------------------------------

Could not connect to J-Link.
Please check power, connection and settings.SEGGER J-Link GDB Server V7.94b Command Line Version

JLinkARM.dll V7.94b (DLL compiled Dec 13 2023 17:05:52)

Command line: -if swd -device XMC4200-F64x256 -endian little -speed 1000 -port 2331 -swoport 2332 -telnetport 2333 -vd -ir -localhostonly 1 -singlerun -strict -timeout 0
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: on
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: XMC4200-F64x256
Target device parameters: none
Target interface: SWD
Target interface speed: 1000kHz
Target endian: little

Connecting to J-Link...
Connecting to J-Link failed. Connected correctly?
GDBServer will be closed...
Shutting down...

 

Please kindly let me know how I can go into debug mode in DAVE IDE.

 

0 Likes
1 Solution
Pradeep_PN
Moderator
Moderator
Moderator
250 sign-ins 100 solutions authored 25 likes received

Hi @hgoo ,

Please make sure to connect the board at the on board debugger side.

The serial device is not getting detected so it seeking an TCP/IP connection. That is because of the J-Link version you have installed, so please delete the current V7.94 and install the older version which is lesser than V7.88.

Please refer to the below thread which  has similar problem for better understanding.

Link : https://community.infineon.com/t5/XMC/Micro-USB-debugger-No-probes-connected-via-USB-for-XMC4400-Pla...

Hope this helps and let me know if you have any further queries.

Best regards
Pradeep.

View solution in original post

0 Likes
1 Reply
Pradeep_PN
Moderator
Moderator
Moderator
250 sign-ins 100 solutions authored 25 likes received

Hi @hgoo ,

Please make sure to connect the board at the on board debugger side.

The serial device is not getting detected so it seeking an TCP/IP connection. That is because of the J-Link version you have installed, so please delete the current V7.94 and install the older version which is lesser than V7.88.

Please refer to the below thread which  has similar problem for better understanding.

Link : https://community.infineon.com/t5/XMC/Micro-USB-debugger-No-probes-connected-via-USB-for-XMC4400-Pla...

Hope this helps and let me know if you have any further queries.

Best regards
Pradeep.

0 Likes