Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

User10870
Level 1
Level 1
Hi There

I’m having the following issues with code debug using Dave 3 (Version: 3.1.10 Installer build : 2014-05-23)

The main issue is that I can’t step-through or use breakpoints on the source. I can load the code and step through in disassembled mode with debug level (minimal –g1) set. When I try to up the debug level (to –g/-g3) I get the following error:

1671.attach

I have set up a new basic sample project in DAVE and I can set the debug level here and I can step through the code as expected.

Any ideas what the issue might be?

Best Regards

Tony
0 Likes
1 Reply
Travis
Employee
Employee
First like received
Hi Tony,

No ideal on this, maybe you can upgrade to DAVE4 and give it another try.

Best Regards
Travis
0 Likes