my first post in this forum and sorry my english is not very well.

My problem is the ADC on XMC2 Go (XMC1100). I have dowload the ADC004_Example1_XMC11 from here and change the pin in IO001/0 to 2.9. Then have connect with a wire the pin 2.9 to pin 3.3v. After compiling and runnung i cannot read the convertet values on "Result.Result" variable in DAVE3-Debugger. It is always "0"(zero). I have tried in free-run and single-step mode.
Secondary i have the "Result.Result" send via serial to PC. It is this same problem. 😞

Now i can't think any further myself. I have tried everything. Please, can you help me, where is the error? 🙂


0 Likes
2 Replies
Not applicable
Hí Nico,

longri wrote:
My problem is the ADC on XMC2 Go (XMC1100). I have dowload the ADC004_Example1_XMC11 from here and change the pin in IO001/0 to 2.9. Then have connect with a wire the pin 2.9 to pin 3.3v. After compiling and runnung i cannot read the convertet values on "Result.Result" variable in DAVE3-Debugger. It is always "0"(zero). I have tried in free-run and single-step mode.
Secondary i have the "Result.Result" send via serial to PC. It is this same problem. 😞


I think the problem is that you did not enable the result interrupt. Please try this: Right-click on the ADC004/0 app, switch to the "Interrupts" tab and check "Enable at Initialization" for the "Result Event".

--
Stephan
0 Likes
Not applicable
Hi Stephan,

thank you for your answer. This was the problem :). Now running.

Nico
0 Likes