Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
Hi all,

I am currently configuring Slice 0 and Slice 1 of CCU4 unit for capturing in timer concatenation mode.
As far as I understand, the process is the following:
-Configure Slice 0 as capture, trigger the events for capturing the signals. Timer concatenation bit 0.
-Configure Slice 1 as capture, Timer concatenation bit 1.
However, I am not able to increase Slice 1 timer counter.
According to the RM, once you set the timer concatenation bit to 1 in Slice 1 it should be configured as Slice 0.
Have I misses any step?
In XMCLib this is the process:
/*
* CCU40 - Slice 0 configuration - Capture Conf
*/

/* Initialize the Slice */
XMC_CCU4_SLICE_CaptureInit(SLICE0_PTR, &capture_config);

XMC_CCU4_EnableShadowTransfer(MODULE_PTR, \
(uint32_t)(XMC_CCU4_SHADOW_TRANSFER_SLICE_0| \
XMC_CCU4_SHADOW_TRANSFER_PRESCALER_SLICE_0));


XMC_CCU4_SLICE_Capture0Config(SLICE0_PTR, XMC_CCU4_SLICE_EVENT_0);
XMC_CCU4_SLICE_ConfigureEvent(SLICE0_PTR, XMC_CCU4_SLICE_EVENT_0, &capture_event0_config);


XMC_CCU4_SLICE_Capture1Config(SLICE0_PTR, XMC_CCU4_SLICE_EVENT_1);
XMC_CCU4_SLICE_ConfigureEvent(SLICE0_PTR, XMC_CCU4_SLICE_EVENT_1, &capture_event1_config);

/* Get the CCU4 slice out of idle mode */

XMC_CCU4_EnableClock(MODULE_PTR, SLICE0_NUMBER);

/* Start the CCU4 Timer */

XMC_CCU4_SLICE_StartTimer(SLICE0_PTR);

/*
* CCU40 - Slice 1 configuration - Timer concatenation
*/

XMC_CCU4_SLICE_CaptureInit(SLICE1_PTR, &capture_timer_concatenation_config);

XMC_CCU4_EnableShadowTransfer(MODULE_PTR, \
(uint32_t)(XMC_CCU4_SHADOW_TRANSFER_SLICE_1| \
XMC_CCU4_SHADOW_TRANSFER_PRESCALER_SLICE_1));

/* Get the CCU4 slice out of idle mode */

XMC_CCU4_EnableClock(MODULE_PTR, SLICE1_NUMBER);

/* Start the CCU4 Timer */

XMC_CCU4_SLICE_StartTimer(SLICE1_PTR)


Also, is there any XMCLib example on this?

Thx
0 Likes
1 Reply
Not applicable
Besides I am using Slice 3 for counting configuration on POSIFx.OUT2.
According to the Errata Sheet, the timer concatenation in CCU8 does not work when specifying an external count resource. But I am using CCU4,
is this the reason it does not work for me?
0 Likes