Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
u-s
Level 4
Level 4
Distributor - Macnica (Japan)
50 sign-ins 25 replies posted First like received
Hi,

I want connect the four XMC4800 devices at using JTAG chain.
What points do you think I should be careful about?

For example
- Whether a buffer is needed
If need the buffer. Could you tell me, add buffer to where and a specifications of buffer?
- Do I need to change the pull-up and pull-down resistance constants according to the number of devices?

Thank you.
0 Likes
3 Replies
jferreira
Employee
Employee
10 sign-ins 5 sign-ins First like received
Hi,

The following pins has internal pull resistor:
- TRST: Internal pull-down
- TMS/SWDIO: Internal pull-up
- TCK/SWCLK: Internal pull-down

External pull resistor in the range 4.7K to 10K are optional.
Debug probes like ULINK2 provides the required buffering.
0 Likes
u-s
Level 4
Level 4
Distributor - Macnica (Japan)
50 sign-ins 25 replies posted First like received
Hi,

Can your J-LINK probes (Infineon KIT_XMC_LINK_SEGGER_V1 ) support multiple ARM chain connection by JTAG?

Best Regards,
Xingwei
0 Likes
SudheeshK
Moderator
Moderator
Moderator
250 sign-ins First question asked 750 replies posted
Hello,

Yes, our kit KIT_XMC_LINK_SEGGER_V1 will support multiple devices on JTAG chain. As you can see from the user manual, KIT_XMC_LINK_SEGGER_V1 debug probe is based on SEGGER J-Link debug firmware. So, we suggest you to refer SEGGER documentation for more details.

Thanks and Regards,
Sudheesh
0 Likes