Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Not applicable
Hello,

i got a XMC4500_45A_V3 General Purpose Kit with the COM Exp. Board.

I would like to Flash it with the ASC Bootloader terminal Programm, but the COM Board only has a RS485 and a CAN Interface.
My PC only has RS232.

It is possible to connect it to my PC anyway or do i need an apdater 485->232?

Thanks a lot!
1 Reply
Not applicable
Hi Hissi,

The connector pin out is different from RS485 and RS232.
So I don't think you can use directly with RS232.

Does your PC have USB port? Since you using V3 board, the board provide virtual COM port.
You can use it to connect the board with your terminal program.

rgds,
Rou
0 Likes