Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Not applicable
Hi,

I want to use the XMC1400 with ASC BSL timeout option. According to the datasheet i should be able to configure the timeout with x*0.333s where x is the BSLTO of the BMI register.

By trial and error i found out that in reality i get the following timeout: 1.5s + x*0.5ms (i tried all possible values of BSLTO and measured the boot time). Can someone confirm this? Is this a silicon bug or an error in the datasheet?

For our application we need the 333ms option, a minimum boot time of 2 seconds is too large.

Thanks!
0 Replies