Not applicable
Nov 29, 2016
07:26 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 29, 2016
07:26 AM
Hi,
I want to use the XMC1400 with ASC BSL timeout option. According to the datasheet i should be able to configure the timeout with x*0.333s where x is the BSLTO of the BMI register.
By trial and error i found out that in reality i get the following timeout: 1.5s + x*0.5ms (i tried all possible values of BSLTO and measured the boot time). Can someone confirm this? Is this a silicon bug or an error in the datasheet?
For our application we need the 333ms option, a minimum boot time of 2 seconds is too large.
Thanks!
I want to use the XMC1400 with ASC BSL timeout option. According to the datasheet i should be able to configure the timeout with x*0.333s where x is the BSLTO of the BMI register.
By trial and error i found out that in reality i get the following timeout: 1.5s + x*0.5ms (i tried all possible values of BSLTO and measured the boot time). Can someone confirm this? Is this a silicon bug or an error in the datasheet?
For our application we need the 333ms option, a minimum boot time of 2 seconds is too large.
Thanks!
- Tags:
- IFX
0 Replies