Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Not applicable
Hi All,

Is it possible in data reduction mode to have more than 4 samples? Or is that a hard limit? Could one somehow use the fifo to trigger a interrupt when it is full and then read out all the data, this should increase the number of samples one can take right?

regards,
Enigma
1 Reply
Travis
Employee
Employee
First like received
Is it possible in data reduction mode to have more than 4 samples?

Max, is 4 result values.


Could one somehow use the fifo to trigger a interrupt when it is full and then read out all the data, this should increase the number of samples one can take right?

Sorry that the FIFO does not behave this way (disappointed :(). If I remembered correctly, every result received will triggered an interrupt.

http://www.infineonforums.com/threads/3781-XMC-4500-VADC-how-use-the-FIFO-buffer-to-reduce-the-CPU-l...
0 Likes