Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
summer-916
Level 1
Level 1
5 sign-ins First reply posted First question asked

您好,我使用XMC1302 MCU,需要采集内部参考电压值作为ADC转换成功的基准,要求对外部硬件不做改动只做软件修改,请问下该怎么配置或者提供例程参考下?

0 Likes
1 Solution

我在链接的帖子回复了这个问题,你看一下是否满足你的要求:

 https://community.infineon.com/t5/XMC/xmc1300-Broken-Wire-Detection/td-p/492034

View solution in original post

0 Likes
8 Replies
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

1:转换成功了,可以有event去反馈成功。

2:关于ADC的内容,可以参考附件的连接:

LinglingG_46_0-1694056134914.png

 

https://www.infineon.com/cms/en/product/microcontroller/32-bit-industrial-microcontroller-based-on-a...

0 Likes

采集内部参考电压的目的:

1、电压恒定,每次采集到的值偏差小,不受外界影响

2、反馈转换成功,怎么确认转换值是正确的

另能否提供xmc1302的UL 60730中相关的AD测试参考源码

0 Likes

ADC可以读出参考电压的值吗,该如何操作?

0 Likes

1:根据我的理解,xmc1302是不能从内部读reference的电压。

2:你读一个电压值,并且通过万用表测量,看是否一致来判断读取是否成功。

3:你说的UL 60730 是从哪里看到的?

4:你采集参考电压目的是什么?

0 Likes

1、采集参考电压目的是作为AD转换器出错导致转换值错误和ADC无法切换采样通道判断

2、目前我司产品正在进行UL认证,需要对ADC进行测试

3、寻求该MCU方案ADC过认证方法或者案例

0 Likes

1:你不确定你AD的采样是否正确,这个问题是基于什么前提问出来的呢?

   你说的无法切换通道的问题是否是代码中实际发生的呢?您能否把你的问题详细描述一下。

我的理解是单片机会按照代码设计的逻辑去运行,一般情况下不存在采集错误以及通道不能切换这样的情况。

2:关于认证的内容你可以参考这个链接:

https://www.hitex.com/tools-components/software-components/selftest-libraries-safety-libs/iec-60335-...

https://community.infineon.com/t5/%E7%9F%A5%E8%AF%86%E5%BA%93%E6%96%87%E7%AB%A0/%E5%A6%82%E4%BD%95%E...

3:根据我的理解XMC1302不能从内部读参考电压的值,但是你可以从外部将一个管脚接到vdd来判断你采样的正确性。

 

0 Likes

Broken Wire Detection:This feature can be used to detect a broken connection to a sensor. If there is continuous conversion of a sensor voltage and the connection with the sensor is interrupted, the conversion results become the precharged value (VAREF or VAGND) instead of the expected sensor value。

文档中有介绍配置成断线检测,是否可以稳定检测到内部VAREF值。有无这个检测的配置例程源码?

0 Likes

我在链接的帖子回复了这个问题,你看一下是否满足你的要求:

 https://community.infineon.com/t5/XMC/xmc1300-Broken-Wire-Detection/td-p/492034

0 Likes