All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
In the end, the target array is still all zeros
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/cyt4fbb7-%E4%BD%BF%E7%94%A8mdma%E5%A4%8D%E5%88%B6%E6%95%B0%E7%BB%84%E6%B2%A1%E6%9C%89%E6%88%90%E5%8A%9F%E6%98%AF%E4%B8%BA%E4%BB%80%E4%B9%88/td-p/724114
Show LessHello,
Can you tell me how to update the firmware on the CYPD2119-24LQXI via USB?
Regards.
Dear Forum:
I know that
The Hex file generated by the Modus Tool box IDE follows the Intel Hex File format which is supported by the Cypress Programmer.
from the following title.
https://community.infineon.com/t5/PSoC-6/PSoC-programmer-parsing-failure/td-p/716946
I want to confirm that
Which IDE can generate hex file used by PSoC programmer?
Thank you.
Show LessHello,
I want to read the 1YN Bluetooth transmit power and write to it. How can I do this with the `hcitool`?
I'm using CYW4343A2_001.003.016.0031.0000.1YN.hcd firmware.
As far as I know CYW43439 has a maximum TX power of 8dB. If so is the following output wrong?
# hcitool -i hci0 cmd 0x08 0x004b
LE Read Transmit Power (0x08|0x004b) ncmd 1
Status: Success (0x00)
Min Tx power: -16 dBm
Max Tx power: 12 dBm
Thanks for all the help,
Mesih
Show LessHi All,
I have a question related to SCR_XRam and SCR_IRam.
The question: How to know whether the SCR_XRam and SCR_IRam are initialized or are not initialized in startup code?
Thanks.
Show LessFrom a linux system, I want to read back the configured program image from a CYC65215 part and check that its CRC is correct -- assuming it has an appended CRC. Does the image have a CRC? Is the CRC generated using a known algorithm with a standard polynomial? If so, which polynomial?
Show LessAre there available instructions or guidance on connecting the BGT60TR13C development kit to a jetson orin nano? Or a way to compile the sdk for the jetson? Following the "Building SDK from source code" in the RFS SDK Documentation in the radar_sdk didn't work for compile or install using python wheel.
Show LessHi
I am building a BLE remote controller. It should respond to user entry and send a command via BLE to the receiver, both are PSOc6.
What is the best practice to reduce power consumption ?
I read the PSoC design documents for low power, but there is still some confusion. The options are to put in deep sleep either CM0+ and/or CM4 until a user entry is detected using GPIO ISR, then it wakes up to resume the connection and send the BLE packet.
What is the best practice ?
Thanks
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023