All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Battery Management ICs
Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.
Featured Discussions
I am looking for a Power MOSFET. I need a Silicon (Si) transistor with high Vds >500V, but I don't know how to find the transistor I need. The list on the website doesn't state transistor material. Please help.
Show Lesshi
i want to use the SCR in order to reduce the power consumption , and meet some block point. please check state flow bellowing :
if SW switch to SCR domain to execute, which position will sw execute next after wake up source login and exit from SCR domain ?
Step A (step A as the SW first code after reset )? or back to Step B?
Show Less
i'm trying SPI_CPU_1_KIT_TC334_LK.. I've joined SPI_A to SPI_B (confirmed on schematic for dev kit - - i hope).
when the code runs i dont have an LED on which says the data has transfered ok -- 😞 .. sad face .
i've run it a few times and set a break point . plus used a logic analyser ..
if i disconnect the MISO / MOSI lines i receive no data .. so i know the SPI slave is getting data.. ..
i've added this line , but nothing has changed ..
spiSlaveConfig.base.mode = SpiIf_Mode_slave; /* Configure the mode */
into the init config for the slave module..
i will continue to look but if anyone has seen this before.....
Where are CAD models for QDPack.
There are .pdf files at https://www.infineon.com/cms/en/product/packages/PG-HDSOP/PG-HDSOP-22-1/ These are NOT CAD models.
STEP form would be preferred.
Greg
Show LessMy radar is Distance2GoL.
I reconfigure the firmware in config.h, make the one frame is 40ms, each frame has 10 pulses, and each pulse lasts 2ms.
First when I charge the board and use OSC to watch it's TX_EN, everything is finr just like I set. Here is the picture of the TX_EN:
But, when I start use matlab to acquire the raw data, when I run the matlab code, it has been changed.
Here is the TX_EN when I start to rum the matlab code:
Please tell me why this matlab code just for acquire the raw data will affect the radar, what should I do to modify the matlab code?
Show LessDear Team,
I want to know the difference between DAP miniwiggler and XMC_LINK_SEGGER_V1.
Hi support,
I would like to set-up a UART connection on my NAC1080 using the GPIO0 and GPIO2 in order to communicate with my PC the messages that the NAC1080 will be sending.
I've been reviewing the uart_drv.h library you have available and what I can't see is how the data transmission works.
There's a function called "transmit_bytes()" that send the Tx buffer data, but where's the Tx buffer?
How could I edit the data on that buffer to be able to send the desired message?
Regards,
-K
Show Less
AN84868 is followed to implement using CX3 to configure FPGA. To be able use the FPGA configuration utility tool, descriptors are the same for AN84868 for FPGA configuration application firmware. After FPGA configuration, firmware switches to CX3 UVC application. FPGA configuration part is good, after switching to UVC application, video streaming is also good. Yet, UART is not able to send out debug information anymore in UVC application. UART debug works during FPGA configuration and printout information on data count for FPGA configuration process.
IO matrix configuration is the same for FPGA configuration application and for UVC application, i.e. I2C, SPI and UART peripherals are all enabled.
I am using GPIO 48 to 49 as the UART tx and rx.
What could be the problem?
Thank you for help in advance.
Show Less
Hello,
I open this issue to fix the problem previously explained here:
https://community.infineon.com/t5/XMC/XMC-usic-end-of-transmission/m-p/670732#M14418
as per requested, I attach the project I am using.
Best regards,
Lander
Show Less
Hi all,
I am looking for Ble module with is able to pass immune test 10V/m.
Standard modules passed basic immune test only for 3V/m
Do you have any information which of the IFX modules is able to pass 10mV?
BR, thx
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023