All Forums
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Featured Discussions
I reconfigure the firmware in config.h: I just modify the bandwidth into 0MHz ,I try to transmit signle tone with my board.
And I also flash the new .hex file inro my board successfully with XMC Flasher.
When I reconnect my board with new FW into my PC, it's LED just like this, only one yellow LED lighting
And when I open GUI, it show no Device connected, and my matlab code also can't run:
Then how can I know this radar still work and really the bandwidth is 0MHz. And if it's still working, I want to extraxt raw data with my matlab code? How can I modify the original code? I really need help, thanks!
Show Less
How to interpret the .npy files that we get in the Radar Fusion GUI. I used the np.load to load the contents of the array( image attached below),the shape of the array is correct, but i am not able to understand what the contents are? Is the contents of .npy file the raw ADC data or it is in byte format?
Show Less
Hi,
is there any solution or workaround available to install miniprog3 drivers on Windows 11 arm based machines, to be able to use the latest PSoC Programmer.
This is also related to:
https://community.infineon.com/t5/PSoC-4/Has-anyone-successfully-used-miniprog3-with-an-Arm-based-host/m-p/378995
Thanks and best regards,
Rico
Hello,
How can I modify the MultiCAN example code for Aurix TC265 to enable transmission of CAN messages over a CAN channel using "Normal Mode" instead of "LoopBack" mode?
Currently on the Aurix website I can not find single example explaining this. Please provide an example that can help me develop the CAN driver.
Kind regards,
Yashaswi Dhiman
Hi,
I'm Trying to implement Hall in IMC102T with Hall as a drive input, motor tries to run but its not running.
If anyone could suggest a solution for this it would be helpful thanks in advance
I had attached MCE wizard configuration file for your reference
Show LessHello! I would like to ask about the Kelvin structure IGBT used in air conditioner PFC, do I have to isolate the Kelvin ground E2 from the ground and E1 of the driver chip? Is it OK if I use a normal bottom-side gate driver?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/%E5%BC%80%E5%B0%94%E6%96%87%E7%BB%93%E6%9E%84%E7%9A%84IGBT%E6%8E%A5%E5%9C%B0%E9%97%AE%E9%A2%98/td-p/717161
Show LessHello.
Please advise if there are any code routines for all four use cases in this document. AN226043 - How to use sound subsystem in TRAVEO T2G family
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/Sound-subsystem-in-TRAVEO-T2G/td-p/717156
Show LessHi~
I'd like to import sameple application named 'Hello Sensor ' from based on CYW20706 to CYBT-343026-01
Because there is no sample applicaion which has same name in CYBT-343026-01
After installing sample application, I tried to exchange BSP from CYW20706 to CYBT-343026-01.
I found some decription indicates successful, But some otheres were not.
Operation is okay after build and flash. But I'm still curious whether it is really okay or not.
Please make me sure it
I attahced error code picture
Many thanks
BRs
Daniel Lim
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023