- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am trying to configure the CYBT-343026-01 BLE module for CYSPP mode. I am experiencing what I believe is unexpected behaviour in peripheral mode.
My setup is:
CYBT-343026-01, CYSPP (pin 22) => GND, LP_MODE (pin 4) => VDD.
On initial bootup, the module behaves as expected - passing all data transmitted to characteristic handle 0x11 to my serial terminal (see below)
Once I disconnect this terminal, the module re-enters API mode (see below)
This is happening even though I believe have disabled API mode in hardware by grounding the CYSPP pin. If I reconnect to the module, all data is now transmitted through the API mode UART interface (all data now encapsulated with "@E,...,D=data etc) which I would ideally like to avoid.
Would anyone please be able to let me know what is incorrect with my setup or thinking?
Any help would be greatly appreciated. Thank-you.
Solved! Go to Solution.
- Labels:
-
Wireless
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please try to use the latest FW which should be 1.2.29 and see if the problem still happens.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Additionally, after about a minute after the first disconnection (and if I haven't re-paired) I receive the following API mode string "@E,000E,ASC,S=00,R=03" which suggests that advertising is being turned off due to a CYSPP state change? But I have left the CYSPP grounded the entire time?
/QFV output: "@R,002C,/QFV,0000,E=01010E06,S=05020016,P=0103,H=D1" which I believe is FW version 1.1.14 build 6 if this helps
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please try to use the latest FW which should be 1.2.29 and see if the problem still happens.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Owen,
Thanks for your response. Is there documentation that you could point me to that provides step-by-step instructions on how to update device firmware?
Thanks again!
Lachlan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I attempted to update firmware OTA.
I used the most recent EZ Serial FW file at https://www.cypress.com/documentation/software-and-drivers/ez-serial-ez-ble-module-firmware-platform (ezserial_343026_release-CYBT_343026_EVAL-rom-ram-Wiced-release.ota.bin) and the "WsOtaUpgrade.exe" included in the WICED-Studio 6.6 release. I followed the steps provided in the User Guide in the section "Device Firmware Update Examples".
1. Paired to the CYBT-343026-01 module on my computer
2. Run "WsOtaUpgrade.exe ezserial_343026_release-CYBT_343026_EVAL-rom-ram-Wiced-release.ota.bin"
3. Followed the prompts to update the firmware (see below, includes output from serial connection during update)
The module is now unresponsive in API mode and CYSPP mode, and I cannot discover any "EZ-Serial" devices with bluetooth scanning. Please advise if there is any way to recover this module or if there is something simple (like a different baud rate?) that changes between 1.1.14 to 1.2.29 that would explain this
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Owen,
I ordered an EVAL board with the CYBT-343026-01 module on it and I can confirm that CYSPP mode works as is specified in the datasheet with firmware version 1.2.29.
I now have issues with API mode on this board and I will try to continue to recover my previous devices, but for the purposes of this question updating to firmware version 1.2.29 solved it.
Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please use the module programmer to program the device: https://community.cypress.com/t5/Knowledge-Base-Articles/WICED-Module-Programmer-User-Guide-KBA22506...
Then program the file ezserial_343026_release-CYBT_343026_EVAL-rom-ram-Wiced-release.hex from here: https://www.cypress.com/documentation/software-and-drivers/ez-serial-ez-ble-module-firmware-platform
Please check the FW version after the program with the boot log.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for your response. I have tried to follow the steps at the link attached using the WICED Module Programmer. I have a USB->UART bridge which is connected to the HCI UART RX and TX pins on the 343026-01 module.
I am attempting to upload the .hex file you have suggested, but the program is erroring with:
08-07-2021 19:05:54.628: WICEDModuleProg: Running test program.
08-07-2021 19:05:54.631: WICEDModuleProg: ToggleComponentsByRunningStatus@2 - Run - Stopped - False
08-07-2021 19:05:54.757: ProgramManager: Selecting_DUT 1/8
08-07-2021 19:05:54.761: ProgramManager: Running_test_program 1/1
08-07-2021 19:05:54.812: Prog[0]COM12 : Write HCI Cmd (COM12): 01 03 0C 00
08-07-2021 19:05:55.327: Prog[0]COM12 : Soft-Reset Fail COM12
08-07-2021 19:05:55.328: Prog[0]COM12 : Failed to reset on baudrate = 115200
08-07-2021 19:05:55.331: Prog[0]COM12 : Failed to reset DUT
08-07-2021 19:05:55.337: ProgramManager: ---->SetResult [1,1] = TestFailed
COM12 is my USB->UART connection. I am assuming the module is running at 115200 baud but have tried all to be sure. I have CTS flow control off.
Is there anything I am missing?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You should program the device with flow control enabled. Please connect the cts and rts pin.
Then program the device under recover mode.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Owen,
Sorry I should’ve said - I performed the reset and recover steps as specified. I grounded both the XRES and SPI2_MOSI pins, and then released the SPI2_MOSI pin, followed by XRES.
My UART->USB does not have cts and rts pins unfortunately, so I cannot do this with my current hardware.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The flow control of HCI UART must be enabled. It is hardware controlled.
Please find a USB to UART tool with CTS and RTS. Then try to program the device again.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Owen, do you think it’s likely that the OTA firmware error has more or less bricked the module?