Wireless Connectivity Forum Discussions
Browse the Community
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
AIROC™ Wi-Fi MCUs
AIROC™ Bluetooth
Featured Discussions
Hello,
We are doing Bluetooth regulatory tests for our product with a CYW43353 chip. The CYW43353 datasheet says that it supports single frequency carrier-wave transmission. We would like to transmit on channel 38. Can we use hci commands to achieve it? I didn't find any vendor specific command for this feature.
Could you please give us some guidance on this? Thank you.
Show LessDear Support Team
There isn't a Flash option in the below picture filter. We were looking for a dual band WiFi SOC or a dual band WiFi&BLE combo SOC with 16MB Flash and supporting IPv6, and can be supplied by battery, and supporting keep sleep for sometime and keep wake up for sometime. Could you please help to recommend us a part number for reference? Many thanks.
Show Less
Hi,
I am using miniProg4 debugger with CYW20835M2EVB-01 EVK and studied attached file. But got error log "cannot read IDR". there is detail log as below. Any idea how to fix it?
Log:
Started by GNU MCU Eclipse
Started by GNU MCU Eclipse
Open On-Chip Debugger 0.11.0+dev-4.4.0.2134 (2022-09-08-13:07)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
adapter speed: 10000 kHz
kitprog3 set_latest_version: C:/Infineon/Tools/ModusToolbox/tools_3.0/fw-loader 2.40.1241
Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.
cortex_m reset_config sysresetreq
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : Using CMSIS-DAPv2 interface with VID:PID=0x04b4:0xf151, serial=0A1D198800121400
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: JTAG supported
Info : CMSIS-DAP: Atomic commands supported
Info : CMSIS-DAP: FW Version = 2.0.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : KitProg3: FW version: 2.40.1241
Info : KitProg3: Pipelined transfers enabled
Info : KitProg3: Asynchronous USB transfers enabled
Info : VTarget = 3.289 V
Info : clock speed 10000 kHz
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
Error: DAP 'CYW20835B1.cpu' initialization failed (check connection, power, transport, DAP is enabled etc.)
Austin
Show LessAs noted in another recent question: https://community.infineon.com/t5/Bluetooth-SDK/a2dp-sink-cant-t-connect-to-20719-a2dp-source/td-p/330401 the Watch Example provided as reference code for A2DP implementation seems to have problems with the connection sequence, and it appears that the code does not actually perform to the Bluetooth Specification. Can you explain the apparent deficiencies or provide examples of compliant code?
As noted in the referenced post above, the connection sequence always seems to fail for a previously paired device. And we do not seem to be able to get SBC output to play on Airpods at all.
Show LessHow to configure CYW43012 in different power modes. I'm using CY8CKIT-062S2-43012 and I've used switching power modes example in ModusToolbox but it is configuring the MCU in different power modes, How can I configure the chip CYW43012 in different power modes
Show LessHow to configure CYW43012 in different power modes. I'm using CY8CKIT-062S2-43012 and I've used switching power modes example in ModusToolbox but it is configuring the MCU in different power modes, How can I configure the chip CYW43012 in different power modes
Show Lessi am use cyw43455 as a ap on linux, i want to use wl util to config the cyw43455 as AP on 2.4G, but i see the channel config is fail, the channel is always "11", even i try to config as channel "1" or "6". below is my wl command list
wl64s down
wl64s ap 1
wl64s wsec 0
wl64s wpa_auth 0
wl64s band b
wl64s country DE
wl64s bw_cap 2g 0x3
wl64s chanspec -c 6 -b 2 -w 20 -s 0
wl64s nrate auto
wl64s frameburst 1
wl64s up
wl64s ssid CMW-AP
and the firmware version is as below
./wl64s ver
1.28 RC0.0
wl0: Apr 15 2021 03:03:20 version 7.45.234 (4ca95bb CY) FWID 01-996384e2
Regards,
Jason
Show Less
In my project, I also need a key Bluetooth, which requires HSM function. The specific requirements are as follows:
Certification requirements :AEC-Q100
Bt Freq: 2.4G RF transceiver compatible with Bluetooth 5.0Low Energy
-40℃-105℃
1 SPI
1 UART
>512K FLASH
3.3V
HSM.
Is there a suitable product recommendation?If not, is there a relevant product plan? Thanks!
Show LessHi,
Is the CYBT-413055-02 module supports for audio communication?
like HFP / HSP, A2DP : Audio streaming, and AVRCP profiles.
I am not able to see the examples related to this profiles.
Thanks & Regards,
Srihari
Show Less
Hi,
I want to convert my CYBT-4803056 module to EZ-serial but firmware as per knowledge base I downloaded the WICED_MOD_Prog_v1.5.19.102.zip but when opened I found it did not support CYBT-483056 board.
Please guide me how I can program this in CYBT-483056 board.
Thanks in advance.
Prasad
Show Less