Wireless Connectivity Forum Discussions
Browse the Community
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
AIROC™ Wi-Fi MCUs
AIROC™ Bluetooth
Recent discussions
Good morning,
We are using a CYW4343W based product (Laird Sterling LWB 450-0152) in our product and need to re-certify the wireless part.
Following the https://www.lairdconnect.com/documentation/sterling-lwb-certification-guide manual, I asked Laird support to get the manufacturing firmware. In order to give me the firmware they told me I have to sign an NDA with Cypress asking this comunity.
How can we do this ?
Thank you!
Guido
Hi, we are interested in the datasheet for the CYW5557x family, in particular the CYW55573.
Hello,
Is there any I2C example code using GPIO? I used all of pins related I2C interface on CYW920706 for I2S audio path, so need to use GPIOs for I2C interface. think there are some example codes for this application.
Could you please help this stuff?
Thanks for your reply in advance.
Show Lesscan CYW20721 BLE transreceiver will support Below Bluetooth audio profiles
HFP V1.5
A2DP V1.2
AVRCP V1.4
GAVDP V1.2
AVDTP V1.2
SPP V1.2
AVCTP V1.2
Or any other Cypress BLE transreceiver IC.
Show Less
Hello,
We are working on integrating Wi-Fi module Murata Type1 MW LBEE5HY1MW(Cypress CYW43455) with STM32F4 based micro-controller using SDIO interface.
We are looking for SDIO Driver and Murata Wi-Fi driver for STM32F4 based micro-controller (Running FreeRTOS).
anyone here having any reference for the same? or
anyone know where we can get them to integrate it in our system?
It would be also great help if there are any compatible software that we can port on STM32F4 based micro-controller.
Regards,
Dipak Sharma
Show LessDear Cypress.
Our customer want to bridge 3ch Analog audio through CYBT-343026-01.
CYBT-343026-01 ADC connect to 3ch Analog audio, is this possible?
I think CYBT-343026-01 ADC pin 2ch support, is this right?
1ch : BT Audio.
2ch: USB/SD Card
3ch: Voice.
And Is This Streaming operate at the same time Possible?
Thank you.
Show Less
Dear Cypress.
I did set-up for CYW720719-EVB through wiced studio.
but I think not provide A2DP SNK Test demo.
I Used Wicedstudio 6.2.1 and Test through client control tool.
Could you provide A2DP SNK Test demo?
thank you.
Show LessDear Cypress.
Our customer progress BT SIG certification.
But certification company has any question.
they thinks to Module to have HW modified.
They thinks to 3points different Marking for module.
this left picture before version and Right picture now version.
Is this 3points parts diffrent?
if same parts, Could you provide parts information?
Show Less
Hello, I'm using CYBT-213043-MESH 02 cards, and modustoolbox 2.2
I would like to know in which part of the bluetooth code these values are stored, since several devices leave the mesh network and they have to be re-entered manually
Show Less
Hello,
After having read the post "How to Debug CYBT343026EVAL with Modus " I expect that it is possible to use MiniProg4 to debug a CTBT-343026 eval board. I am in the configuration given below :
1- Modus toolbox Version: 2.2.0 Build ID: 2181
2- debug tool "CY8CKIT-005 MiniProg4 " with the configuration given by "Cypress programmer" :
Info : Connected - MiniProg4 CMSIS-DAP BULK-1F1C15C800287400 FW Version 2.10.878
Info : Selected Device: MP4 BULK-1F1C15C800287400
Info : Could not connect to device: MiniProg4/PSoC 61/62/63
Info : Open On-Chip Debugger 0.10.0+dev-3.0.0.665 (2020-03-20-10:13)
3 - Connected to "CYBT-343026-01" as show in the give the attached picture.
4- I have take project "HAL_PUART" given in the "project example creator" and change "ENABLE_DEBUG?=1" build all and flash
I am trying to use MiniProg4 for debugging and IDE is reporting an error (see attached error picture). Does anyone already encounter this problem ?
Thank you in advance for your support
Show Less