Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wireless Connectivity Forum Discussions

Browse the Community

filter icon

Featured Discussions

Sort by:
jtornosm
AIROC™ Wi-Fi MCUs
Using Fedora38 on two systems with BCM4356 802.11ac Wireless Network Adapter I get these messages and WiFi results: Dell Inspiron 660[ 22.813891] brcm... Show More
nobody19
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
What is the maximum tx power for the CYW4373E? When I read it back with the the function "wiced_bt_ble_read_adv_tx_power" it says 12, is that meaning... Show More
gca1
AIROC™ Wi-Fi MCUs
Hi, I would like to modify (increase) the TX power of the WiFi.  IOVAR_STR_QTXPOWER is the correct variable to use for changing TX power? What value ... Show More
cedric_roomz
AIROC™ Wi-Fi MCUs
Hi,  We are waiting on the serial flash support on modustoolbox for the cyw43907. Our aim is to implement OTA and also read /write some data on the fl... Show More
Ostrovsky
AIROC™ Wi-Fi MCUs

The AP sends out beacon as data rate is 6Mbps, and 43012 could not find the AP by scan.

shlim
AIROC™ Bluetooth
Hi~   I'm considering about the CYW20736 chip for suggesting for my custonmer. But, I've found there  is no internal flash. So I need to double-check ... Show More
darsan
AIROC™ Wi-Fi MCUs
I am following exactly as done in a previous forum post as in - https://community.infineon.com/t5/AIROC-Wi-Fi-MCUs/Wifi-driver-fmac-modules-Build-and-bring-up-for-Nvidia-Nano-B01-board/m-p/406356#M2725... Show More
Sean2
AIROC™ Wi-Fi MCUs
在改信道问题上遇到了几个疑问,想请教一下。       1,将国家码改为RUSSIAN_FEDERATION,信道改为44后烧录程序后无法找到WiFi信号。      2,将国家码改为RUSSIAN_FEDERATION,信道改为165后烧录程序后无法找到WiFi信号       3,将国家码改为... Show More
Meet_Modia
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
Hi Team, We have used CYW43439 in our design,  can you share how we can integrate in Linux kernel version 6.1 Also if you can share the NVRAM bin file... Show More
JoJoDucati
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
Dear Infineon,                      Whether the WiFi 6 (CYW55572) support IEEE 802.11p, IEEE 802.11s, or IBSS / Adhoc mode? Thanks.   Show More