- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
When I run the "config_mode" snip and enter a 0 for in the zip code field in the application data webpage, it doesn't show up the next time the page is loaded. The zip field just shows up empty after a refresh. The value is getting saved into the dct. But displaying a zero seems to break whatever code is supplying the dynamic content.
I don't think it's a browser or js bug because the source comes from the http server that way. What can I change to allow a zero to show up in a number field linked to the dct?
- Labels:
-
SPI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please update the ...Wiced/internal/wiced_lib.c.
Below are the changes:
--- a/Wiced/internal/wiced_lib.c
+++ b/Wiced/internal/wiced_lib.c
@@ -54,2 +54,5 @@ uint32_t utoa(uint32_t value, char* output, uint8_t min_length, uint8_t max_leng
int8_t digits_left = max_length;
+ if (value == 0)
+ --digits_left;
+ else
while (value != 0 && digits_left != 0)
Thanks,
Seyhan