Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

tepa_4520591
Level 1
Level 1

Hi ,

We have using cypress wifi chip and integrated wifi driver and wifi HAL. Still WiFi bring up issue.


Dmesg log time: 

dhd_prot_ioctl : return error code-23 below error comes and i was check driver code and it check ifdef and return BCME_UNSUPPORTED rertun code by -23?

Cypress provide any patch overcome for this issue  -23 ?

#define BCME_UNSUPPORTED        

-23/* Unsupported */

[
[2.101205] dhd_prot_ioctl: status ret value is -23
[2.101210] dhd_preinit_ioctls Disable rsdb_mode is failed ret= -23
[2.101213] Firmware up: op_mode=0x0005, MAC=a0:c9:a0:8f:dc:ab
[2.102742] dhd_prot_ioctl: status ret value is -23
[2.102747] dhd_preinit_ioctls Set txbf returned (-23)
[2.103582] dhd_prot_ioctl: status ret value is -23
[2.103585] dhd_preinit_ioctls pspretend_threshold for HostAPD failed  -23
[2.105620] clm version = Cypress.Automotive
[2.105781] Firmware version = wl0: Mar 12 2018 01:06:33 version 9.40.80 (r684423 CY) FWID 01-35ae044b
[2.106165] dhd_prot_ioctl: status ret value is -14
[2.106168] dhd_pno_init: Support Android Location Service
[2.106419] dhd_prot_ioctl: status ret value is -16
[2.106421] dhd_interworking_enable: set wnm returned (-16)
[2.106621] dhd_prot_ioctl: status ret value is -23

logcat log with android HAL and wpa_supplicant:

--------------------------------------------------------------------

05-16 12:58:51.814  1048  1048 I wpa_supplicant: Successfully initialized wpa_supplicant

rfkill errror : rfkill unlock all required ? then below issue resolved?

05-16 12:58:51.979  1048  1048 I wpa_supplicant: rfkill: Cannot open RFKILL control device

05-16 12:58:52.030  1048  1048 I wpa_supplicant: rfkill: Cannot get wiphy information

After that wifi HAL error comes

05-16 12:58:52.086   128   128 E WifiHAL : Failed to register debug response; result = -23 --> Debug_command in WiFI Hal start request response failed ..libnl issue ? because call nl_sock_send_msg.  i have checking send_msg path ?

05-16 12:58:52.088   128   128 D WifiHAL : createRequest Monitor packet fate request

05-16 12:58:52.088   128   128 E WifiHAL : Failed to register get pkt fate response; result = -95

1 Solution
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

hello:

I think you can remove the dhd_preinit_ioctls where return -23 ,  because some chip can't support the features like RSDB, or some functions are not enabled in your debug firmware.

View solution in original post

1 Reply
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

hello:

I think you can remove the dhd_preinit_ioctls where return -23 ,  because some chip can't support the features like RSDB, or some functions are not enabled in your debug firmware.