cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

NiMc_1688136
Contributor II

SDK 6.2.0

CYW43907

FreeRTOS + lwIP

I have been using wiced_tcp_send_packet without any issues until i tried to send larger packets. I then switched to wiced_tcp_send_buffer and it works great in an example application with no TLS but once TLS is added and the packet is large enough to be fragmented, I run into a data_abort exception. The best that I can tell, the problem occurs in wiced_tcpip_common.c, at line 213, during the free call.

        if (enc_buf_allocated == WICED_TRUE)

        {

            free(enc_output_buf);

            enc_output_buf = NULL;

        }

Has anyone seen this?

The packet i was attempting to send was between 1800 and 1900 bytes.

0 Likes
1 Solution
PriyaM_16
Moderator
Moderator

Have you tried increasing the packet pool size:

GLOBAL_DEFINES += TX_PACKET_POOL_SIZE=xx \

                     RX_PACKET_POOL_SIZE=xx \

                     WICED_TCP_TX_DEPTH_QUEUE=xx \

                     WICED_TCP_RX_DEPTH_QUEUE=xx

Choose xx to be a value greater then your current value.

View solution in original post

3 Replies
PriyaM_16
Moderator
Moderator

Have you tried increasing the packet pool size:

GLOBAL_DEFINES += TX_PACKET_POOL_SIZE=xx \

                     RX_PACKET_POOL_SIZE=xx \

                     WICED_TCP_TX_DEPTH_QUEUE=xx \

                     WICED_TCP_RX_DEPTH_QUEUE=xx

Choose xx to be a value greater then your current value.

NiMc_1688136
Contributor II

Thanks for the response Priya. I have not made the queues/pools larger through my makefile so the application is using the default values.

This is simple enough for me to test it today. I will follow up with the results.

0 Likes
PriyaM_16
Moderator
Moderator

Hello,

Were you able to send large packets by increasing the packet pool size?

0 Likes