Hi,
I am working on Murata1LD board
In my code, call to wiced_aws_disconnect causes program to hang. I suspect a memory leak. I followed the solution in below thread. But the issue is not yet solved.
Whenver , wifi connection is interrupted, the code hangs there. Apart from the solution mentioned in above thread, is there anything to be done.
Thanks,
Binsy M S
An issue was reported where there was a memory leak after multiple connections and disconnections to the AWS. Can you do the below changes and see if it fixes the issue?
Add the below lines in /43xxx_Wi-Fi/libraries/protocols/AWS/aws_mqtt.c in the function aws_internal_mqtt_disconnect() after the line ret = wiced_mqtt_disconnect( mqtt );
wiced_mqtt_deinit(mqtt); //Memory Leak fix
free(mqtt); //Memory Leak fix
mqtt = NULL;
Add the below line in /43xxx_Wi-Fi/libraries/protocols/AWS/wiced_aws.c in the function wiced_result_t wiced_aws_deinit( void ) after the tls_deinit
free(g_aws_thing.tls_identity);
Thanks
Hi,
I have already tried the below solution.
Add the below lines in /43xxx_Wi-Fi/libraries/protocols/AWS/aws_mqtt.c in the function aws_internal_mqtt_disconnect() after the line ret = wiced_mqtt_disconnect( mqtt );
wiced_mqtt_deinit(mqtt); //Memory Leak fix
free(mqtt); //Memory Leak fix
mqtt = NULL;
And the other one you mentioned is already present in the files of WICED-Studio-6.4
Add the below line in /43xxx_Wi-Fi/libraries/protocols/AWS/wiced_aws.c in the function wiced_result_t wiced_aws_deinit( void ) after the tls_deinit
free(g_aws_thing.tls_identity);
But the issue is not resolved with these solutions
Thanks,
Binsy M S
Which is the application that you are using?
When does it hang?
Can you give me the steps to reproduce this?
I am trying to develop an application by modifying publisher project in wiced-studio. with qos =1, when it fails to get the publish acknowledgement , wiced_aws_disconnect is called to forcefully disconnect. After this when it again tries to connect , the program gets hung.
/* Published - Check if we want an acknowledgment */
if (qos > WICED_AWS_QOS_ATMOST_ONCE)
{
ret = wiced_rtos_get_semaphore(&event_semaphore, APP_AWS_PUBLISH_ACK_TIMEOUT);
if (ret != WICED_SUCCESS)
{
WPRINT_APP_INFO(("[Application/AWS] Error Receiving Publish Ack(ret: %d)\n", ret));
/* if we are still connected; Force a Disconnect */
if (is_connected)
{
wiced_aws_disconnect(aws_connection);
}
is_connected = 0;
}
}
Thanks,
Binsy M S
I don't seem to be able to reproduce the issue that you are reporting. Can you give out your application and the steps for me to reproduce the issue?