Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
user_2170816
Level 3
Level 3
5 replies posted 5 questions asked First question asked

Hello,

I am trying to upload an image to my hardware with download download_apps. But APP download sometimes it fails and console message is the following:

tools/makefiles/wiced_apps.mk:252: recipe for target 'APP0_DOWNLOAD' failed

make.exe[1]: *** [APP0_DOWNLOAD] Error 1

make: *** [main_app] Error 2

Makefile:220: recipe for target 'main_app' failed

When I took a look at the openocd_log file these are the logs:

Open On-Chip Debugger 0.7.0-dev-00227-g9d47214-dirty (2013-04-16-10:43)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'jtag'

DEPRECATED! use 'adapter_khz' not 'jtag_khz'

adapter speed: 1000 kHz

DEPRECATED! use 'adapter_nsrst_delay' not 'jtag_nsrst_delay'

adapter_nsrst_delay: 100

jtag_ntrst_delay: 100

cortex_m3 reset_config vectreset

post_init_43909_setup

Info : J-Link initialization started / target CPU reset initiated

Info : J-Link V10 compiled Oct  9 2015 20:36:39

Info : J-Link caps 0xb9fe7bbf

Info : J-Link hw version 101000

Info : J-Link hw type J-Link

Info : J-Link max mem block 26488

Error: dummy byte read failed

Error: jlink_usb_read failed (requested=256, result=-107)

Info : J-Link JTAG Interface ready

Info : clock speed 1000 kHz

Info : JTAG tap: stm32f2xxx.cpu tap/device found: 0x4ba00477 (mfg: 0x23b, part: 0xba00, ver: 0x4)

Info : JTAG tap: stm32f2xxx.bs tap/device found: 0x06411041 (mfg: 0x020, part: 0x6411, ver: 0x0)

Info : Selecting JTAG transport command set.

Info : AP INIT COMPLETE

Info : stm32f2xxx.cpu: hardware has 6 breakpoints, 4 watchpoints

target state: halted

target halted due to debug-request, current mode: Handler SVCall

xPSR: 0x4100000b pc: 0x0800d1b6 msp: 0x20010fcc

27856 bytes written at address 0x20000000

downloaded 27856 bytes in 0.455026s (59.784 KiB/s)

entry_address= 536888649

stack_address= 536908240

buffer_size= 16384

pc (/32): 0x20004549

Total write size is 534804

writing 16384 bytes at 4096

target state: halted

target halted due to breakpoint, current mode: Handler HardFault

xPSR: 0x21000003 pc: 0x2000445a msp: 0x20009130

loadimage address 536870940 foffset 0 16384

16384 bytes written at address 0x2000001c

downloaded 16384 bytes in 0.255014s (62.742 KiB/s)

target state: halted

target halted due to debug-request, current mode: Handler SVCall

xPSR: 0x4100000b pc: 0x0800d1b6 msp: 0x20010fcc

Runtime Error: apps/waf/sflash_write/sflash_write.tcl:207: can't read "RESULT(62)": no such element in array

in procedure 'sflash_write_file'

in procedure 'program_sflash' called at file "apps/waf/sflash_write/sflash_write.tcl", line 255

at file "apps/waf/sflash_write/sflash_write.tcl", line 207

I underlined "sometimes" at the very beginning of the post because I realized that when I changed something in the code uploading image is successful. I think that the error could be caused by image size. Is there any comment or solution about issue?

Bests,

Oguz.

0 Likes
3 Replies
JeGu_2199941
Level 5
Level 5
25 likes received 10 likes received 10 likes given

I'm not sure if your issue is related to image size.

Bu if it is, what I will try first is turn off some unnecessary debug prints.

You can try toggling WICED print macros from <wiced_defaults.h>
(And of course the same thing for your own macros)

Or if you're using WIFI and being sure that you won't need TLS, put the below line in your .mk

GLOBAL_DEFINES += WICED_DISABLE_TLS

Or if you use TLS and being sure you won't need some cipher suites, un-define them in <tls_cipher_suites.h>

Basically it's naively "turn off things you don't need".

Please kindly report if the above modification may go wrong in some cases.

Other tricks for reducing code size are also welcomed.

Appreciated.

xavier@candyhouse wrote:

I'm not sure if your issue is related to image size.

Bu if it is, what I will try first is turn off some unnecessary debug prints.

Then you are trying to hide the issue.

If image size might be an issue, try increase the image size to see if it's easier to reproduce.

If yes, that would be helpful for the developers to figure out the real problem.

BTW, I do see such issue sometimes.

0 Likes
AxLi_1746341
Level 7
Level 7
10 comments on KBA 5 comments on KBA First comment on KBA

oguzkerem wrote:

Hello,

I am trying to upload an image to my hardware with download download_apps. But APP download sometimes it fails and console message is the following:

tools/makefiles/wiced_apps.mk:252: recipe for target 'APP0_DOWNLOAD' failed

make.exe[1]: *** [APP0_DOWNLOAD] Error 1

make: *** [main_app] Error 2

Makefile:220: recipe for target 'main_app' failed

I hit similar issue on SDK-3.7.0-7:

tools/makefiles/wiced_apps.mk:244: recipe for target 'FR_APP_DOWNLOAD' failed

make[1]: *** [FR_APP_DOWNLOAD] Error 1

Makefile:286: recipe for target 'main_app' failed

make: *** [main_app] Error 2

apps/waf/sflash_write/sflash_write.tcl:207: Error: can't read "RESULT(134609288)": no such element in array

in procedure 'sflash_write_file'

in procedure 'program_sflash' called at file "apps/waf/sflash_write/sflash_write.tcl", line 255

at file "apps/waf/sflash_write/sflash_write.tcl", line 207

0 Likes