On ThreadX build:
WICED_TLS_MINOR_VERSION_MIN=0 && WICED_TLS_MINOR_VERSION_MAX=0 works
WICED_TLS_MINOR_VERSION_MIN=0 && WICED_TLS_MINOR_VERSION_MAX=1 works
WICED_TLS_MINOR_VERSION_MIN=0 && WICED_TLS_MINOR_VERSION_MAX=2 fails
On FreeRTOS build
WICED_TLS_MINOR_VERSION_MIN=0 && WICED_TLS_MINOR_VERSION_MAX=0/1/2 all fails
For the failure case, sometimes I got join result 1007, and sometimes it just hang.
grsr
The test result is similar to the PEAP test.
So the enterprise security does not work for FreeRTOS+LwIP build at all.
The issue with FreeRTOS has been reproduced. However, I could not reproduce it with ThreadX, TLSv1.2. Please provide your setup details:
Freeradius version
Ubuntu version
Openssl version
Platforms tested
grsr wrote:
The issue with FreeRTOS has been reproduced.
So how is the status now? Does it work in sdk-6.2?
grsr wrote:
The issue with FreeRTOS has been reproduced.
It has been more than 6 months since you replied you can reproduce the issue with FreeRTOS build.
Can you confirm if upcoming 7.0 release will fix this issue?
FYI: When test EAP-TTLS in debug build of freeRTOS build.
I always hit assertion:
pbuf_header_impl (p=0x2000bd62 <memp_memory_PBUF_POOL_RX_base+3410>, header_size_increment=11689, force=0 '\000') at WICED/network/LwIP/ver2.0.3/src/core/pbuf.c:641
641 LWIP_ASSERT("bad pbuf type", 0);
(gdb) l
636 * bail out unsuccessfully */
637 return 1;
638 }
639 } else {
640 /* Unknown type */
641 LWIP_ASSERT("bad pbuf type", 0);
642 return 1;
643 }
644 /* modify pbuf length fields */
645 p->len += header_size_increment;
(gdb) p type
$1 = 139
The variable p->type shows different values in different test.
Something is very wrong in sdk-6.2.1.