- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I've found out that "download_apps" actually doesn't download the firmware to the SPI flash on the BCM4343W_AVN platform. Has anyone experienced anything like this?
Here's my OpenOCD output:
Open On-Chip Debugger 0.10.0-dev-00224-g217aaab-dirty (2016-09-08-15:37)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 2000 kHz
adapter_nsrst_delay: 100
none separate
post_init_43909_setup
Info : Unable to match requested speed 2000 kHz, using 1800 kHz
Info : Unable to match requested speed 2000 kHz, using 1800 kHz
Info : clock speed 1800 kHz
Info : STLINK v2 JTAG v27 API v2 SWIM v6 VID 0x0483 PID 0x3748
Info : using stlink api v2
Info : Target voltage: 3.208372
Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints
26820 bytes written at address 0x20000000
downloaded 26820 bytes in 0.301316s (86.923 KiB/s)
entry_address= 536888685
stack_address= 536907212
buffer_size= 16384
pc (/32): 0x2000456D
Total write size is 383156
writing 16384 bytes at 4096
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x81000000 pc: 0x20005fde msp: 0x20008d7c
loadimage address 536870940 foffset 0 16384
16384 bytes written at address 0x2000001c
downloaded 16384 bytes in 0.178440s (89.666 KiB/s)
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x21000000 pc: 0x20006374 msp: 0x20008c34
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x61000000 pc: 0x200052c4 msp: 0x20008c14
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x41000000 pc: 0x20005540 msp: 0x20008c24
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x61000000 pc: 0x20004a68 msp: 0x20008cf4
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x2100dc00 pc: 0x20005244 msp: 0x20008c1c
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x21000000 pc: 0x200063a2 msp: 0x20008c6c
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x61000000 pc: 0x20004dd2 msp: 0x20008d0c
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x21000000 pc: 0x200063d4 msp: 0x20008d74
****************** Result: Verify after write failed
stm32f4x.cpu: target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x41000000 pc: 0x200063b4 msp: 0x20008d74
===== arm v7m registers
(0) r0 (/32): 0x40000800
(1) r1 (/32): 0x20008D78
(2) r2 (/32): 0x40010000
(3) r3 (/32): 0x00000004
(4) r4 (/32): 0x2000000C
(5) r5 (/32): 0x2000000C
(6) r6 (/32): 0x0000100A
(7) r7 (/32): 0x200068C4
(8) r8 (/32): 0x00000000
(9) r9 (/32): 0x0000100A
(10) r10 (/32): 0x00000000
(11) r11 (/32): 0x2000401C
(12) r12 (/32): 0x00000000
(13) sp (/32): 0x20008D74
(14) lr (/32): 0x200059C7
(15) pc (/32): 0x200063B4
(16) xPSR (/32): 0x41000000
(17) msp (/32): 0x20008D74
(18) psp (/32): 0x00000000
(19) primask (/1): 0x00
(20) basepri (/8): 0x00
(21) faultmask (/1): 0x00
(22) control (/2): 0x00
(23) d0 (/64): 0x0000000000000000
(24) d1 (/64): 0x0000000000000000
(25) d2 (/64): 0x0000000000000000
(26) d3 (/64): 0x0000000000000000
(27) d4 (/64): 0x0000000000000000
(28) d5 (/64): 0x0000000000000000
(29) d6 (/64): 0x0000000000000000
(30) d7 (/64): 0x0000000000000000
(31) d8 (/64): 0x0000000000000000
(32) d9 (/64): 0x0000000000000000
(33) d10 (/64): 0x0000000000000000
(34) d11 (/64): 0x0000000000000000
(35) d12 (/64): 0x0000000000000000
(36) d13 (/64): 0x0000000000000000
(37) d14 (/64): 0x0000000000000000
(38) d15 (/64): 0x0000000000000000
(39) fpscr (/32): 0x00000000
===== Cortex-M DWT registers
(40) dwt_ctrl (/32)
(41) dwt_cyccnt (/32)
(42) dwt_0_comp (/32)
(43) dwt_0_mask (/4)
(44) dwt_0_function (/32)
(45) dwt_1_comp (/32)
(46) dwt_1_mask (/4)
(47) dwt_1_function (/32)
(48) dwt_2_comp (/32)
(49) dwt_2_mask (/4)
(50) dwt_2_function (/32)
(51) dwt_3_comp (/32)
(52) dwt_3_mask (/4)
(53) dwt_3_function (/32)
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Problem solved: it was a hardware wiring problem (caused by an error in the datasheet). More info here:
http://cloudconnectkits.org/forum/topic/feedback-error-datasheet
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Problem solved: it was a hardware wiring problem (caused by an error in the datasheet). More info here:
http://cloudconnectkits.org/forum/topic/feedback-error-datasheet