- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In my application, I have built all images for ota2 with the final one being ota2_manuf_download.
- Built extraction app
- Built ota2_image
- Built otat factory image
- built ota2 manufacturing image (with -debug added to platform).
When I run the application, it fails during wicedfs_init with a -2.
fs_header elements are all 1's.
SDK = 6.2.0
platform_result_t platform_filesystem_init( void )
{
int result;
if ( fs_init_done == 0)
{
if ( init_sflash( &wicedfs_sflash_handle, 0, SFLASH_WRITE_NOT_ALLOWED ) != WICED_SUCCESS )
{
return PLATFORM_ERROR;
}
#if (DCT_BOOTLOADER_SDK_VERSION < DCT_BOOTLOADER_SDK_3_1_2)
/* this SDK does not have apps_locations in bootloader_dct_header_t (platform_dct_header_t for the SDK) */
#else
if ( wiced_framework_app_open( DCT_FILESYSTEM_IMAGE_INDEX, &fs_app ) != WICED_SUCCESS )
{
return PLATFORM_ERROR;
}
#endif /* (DCT_BOOTLOADER_SDK_VERSION < DCT_BOOTLOADER_SDK_3_1_2) */
result = wicedfs_init( 0, read_callback, &resource_fs_handle, &wicedfs_sflash_handle );
wiced_assert( "wicedfs init fail", result == 0 );
fs_init_done = ( result == 0 ) ? 1 : 0;
return ( result == 0 ) ? PLATFORM_SUCCESS : PLATFORM_ERROR;
}
return PLATFORM_SUCCESS;
}
int wicedfs_init ( wicedfs_usize_t base, wicedfs_read_func_t read_func, /*@out@*/ wicedfs_filesystem_t* fs_handle, /*@dependent@*/ void * user_param )
{
wicedfs_filesystem_header_t fs_header;
wicedfs_usize_t bytes_read;
WICEDFS_CHECK_PARAMS ( ( read_func == NULL ) || ( fs_handle == NULL ), -1 );
/* Read the filesystem header */
bytes_read = read_func( user_param, &fs_header, (wicedfs_usize_t) sizeof(fs_header), base );
if ( bytes_read != sizeof(fs_header) )
{
return -1;
}
/*@-usedef@*/ /* Lint: splint does not pick up 'out' annotation of function pointer read_func */
/* Check the magic number and version matches */
if ( ( fs_header.magic_number != WICEDFS_MAGIC ) ||
( fs_header.version != (uint32_t) 1 ) )
{
return -2;
}
/* Save the hardware address of the root directory
* in the filesystem handle for use by other functions
*/
fs_handle->root_dir_addr = base + fs_header.root_dir_offset; /*@+usedef@*/
fs_handle->read_func = read_func;
fs_handle->user_param = user_param;
return 0;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Just to add, if I remove all OTA2 from the build and application, the program will run / debug fine.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content