- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
HI,ALL:
I want to increase bootloader size,and i modify bootapp_link.ld bootloader_link.ld dct_link.ld and dct_only_link.ld as follows:
MEMORY
{
BTLDR_VECTORS (rx) : ORIGIN = 0x08000000, LENGTH = 512
BTLDR_API (rx) : ORIGIN = 0x08000200, LENGTH = 512
BTLDR_CODE (rx) : ORIGIN = 0x08000400, LENGTH = 31K
DCT1_FLASH (rx) : ORIGIN = 0x08008000, LENGTH = 16K
DCT2_FLASH (rx) : ORIGIN = 0x0800C000, LENGTH = 16K
APP_HDR (rx) : ORIGIN = 0x08010000, LENGTH = 512
APP_CODE (rx) : ORIGIN = 0x08010200, LENGTH = 0x6FE00
SRAM (rwx) : ORIGIN = 0x20000000, LENGTH = 96K
}
and modify stm32f4xx_platform.c file about DCT operate:
#define PLATFORM_DCT_COPY1_START_SECTOR ( FLASH_Sector_2 )
#define PLATFORM_DCT_COPY1_START_ADDRESS ( DCT1_START_ADDR )
#define PLATFORM_DCT_COPY1_END_SECTOR ( FLASH_Sector_2 )
#define PLATFORM_DCT_COPY1_END_ADDRESS ( DCT1_START_ADDR + DCT1_SIZE )
#define PLATFORM_DCT_COPY2_START_SECTOR ( FLASH_Sector_3 )
#define PLATFORM_DCT_COPY2_START_ADDRESS ( DCT2_START_ADDR )
#define PLATFORM_DCT_COPY2_END_SECTOR ( FLASH_Sector_3 )
#define PLATFORM_DCT_COPY2_END_ADDRESS ( DCT1_START_ADDR + DCT1_SIZE )
if i modify like this the app can't run,bu moidfy as follows ,the app will work.
MEMORY
{
BTLDR_VECTORS (rx) : ORIGIN = 0x08000000, LENGTH = 512
BTLDR_API (rx) : ORIGIN = 0x08000200, LENGTH = 512
BTLDR_CODE (rx) : ORIGIN = 0x08000400, LENGTH = 15K
DCT1_FLASH (rx) : ORIGIN = 0x08004000, LENGTH = 16K
DCT2_FLASH (rx) : ORIGIN = 0x08008000, LENGTH = 16K
APP_HDR (rx) : ORIGIN = 0x0800C000, LENGTH = 512
APP_CODE (rx) : ORIGIN = 0x0800C200, LENGTH = 0x73E00
SRAM (rwx) : ORIGIN = 0x20000000, LENGTH = 96K
}
STM32F401xD/E Flash module organization table