Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

In the WICED SDK, under the directory Platform/.../, we set the parameter maxp2ga0 to modify transmit power (e.g, for 16 dbm, we set the paramter to 64). When we call the function wiced_wifi_set_tx_power from the application,does it override the initial maxp2ga0  parameter? Or, Does tx_power still remain the same as the initial value in the nvram_file even if we call the function from the application?


Thanks.

0 Likes
1 Solution
SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Hi,

The nvram parameters defined in the .../platforms/<platform>/wifi_nvram_image.h are applied before the application entry thread is created, application_start( ). After WLAN chip initialization, if application makes a call to change parameters of the WLAN chip new value will overwrite the value defined in the wifi_nvram_image.h file.

In your example, the application setting the maxp2ga0 value overwrites the default value defined in the wifi_nvram_image.h file.


Seyhan

View solution in original post

1 Reply
SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Hi,

The nvram parameters defined in the .../platforms/<platform>/wifi_nvram_image.h are applied before the application entry thread is created, application_start( ). After WLAN chip initialization, if application makes a call to change parameters of the WLAN chip new value will overwrite the value defined in the wifi_nvram_image.h file.

In your example, the application setting the maxp2ga0 value overwrites the default value defined in the wifi_nvram_image.h file.


Seyhan