- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
hello
i am try to test LBEE5KL1DX (https://wireless.murata.com/type-1dx.html ) using stm32F429ZI NUCLEO board.
we notice NEB1DX-02 (https://www.futureelectronics.com/p/development-tools--development-tool-hardware/neb1dx-02-future-el... ) has same stm32F429ZI chip with LBEE5KL1DX wifi+BT module
so i am try to test LBEE5KL1DX with my nucleo-F429ZI ("https://www.st.com/en/evaluation-tools/nucleo-f429zi.html ") using WICED studio
i am use NEB1DX-02 firmware,
i am try to download NEB1DX-02 example into nucleo-F429ZI
i am use "scan" example of NEB1DX-02.
i am update directly "scan" example's ".bin" file using ST-LINK but its not working
so i am try to add ST-LINK support in WICED using this link (Adding ST-Link support in WICED )
but it will generate error like
Merge all bin files into a single bin for MSD upload
Downloading Bootloader ...
build\waf.bootloader-NoOS-NEB1DX_02\binary\waf.bootloader-NoOS-NEB1DX_02_PAD.bin
build\NABULA.scan2-NEB1DX_02\DCT.bin_PAD.bin
build\NABULA.scan2-NEB1DX_02\binary\NABULA.scan2-NEB1DX_02.bin
1 file(s) copied.
Location: build/NABULA.scan2-NEB1DX_02/binary/NABULA.scan2-NEB1DX_02.bin_MSD.bin
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading DCT ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading Application ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Resetting target
tools/makefiles/standard_platform_targets.mk:226: recipe for target 'run' failed
make.exe[1]: *** [run] Error 1
Makefile:351: recipe for target 'main_app' failed
make: *** [main_app] Error 2
please suggest me way to test LBEE5KL1DX using nucleo-F429ZI.
my only goal is to test LBEE5KL1DX
with WICAD studio or without WICAD studio
with nucleo-F429ZI or nucleo-F429ZI
All suggestion are welcome
thank you
Solved! Go to Solution.
- Labels:
-
WICED Studio
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You were getting OpenOCD error. And from the logs, we can know the download procedures all failed.
So I would suggest you start by looking into the driver/bridge problems that hold you from downloading the firmware.
Best regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You were getting OpenOCD error. And from the logs, we can know the download procedures all failed.
So I would suggest you start by looking into the driver/bridge problems that hold you from downloading the firmware.
Best regards