- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm using Gedday to connect to an Android device.
Gedday works okay most of the time.
Maybe, 5% of the time the gedday_init(...) call fails. I should be more specific. The call blocks & never returns.
Here's the call:
result = gedday_init(
WICED_STA_INTERFACE,
"WICED_Gedday_Discovery_Example"
);
Any insight is helpful.
Thank you.
Solved! Go to Solution.
- Labels:
-
Wifi+Bluetooth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The issue resolved itself at some point, and the project has moved on since then.
This response is from memory. I'll look at setting time aside to reproduce the issue.
I was having the issue when I was having multiple WICED boards start up at the same time. The WICED boards connect to a control AP along with a PC & an Android device.
Edit: The WICED_RESULT would come back true, but the Android device would never see the advertisement.
The call blocks & never returns. Thanks axel.lin_1746341 for remembering this better than I did.
The issue doesn't appear anymore. There's a more involved "out of box setup" now, and that means that I don't have a whole set of WICED boards doing their setup at the same time. That might be a red herring (all the boards starting at the same time).
Thanks.