failed debug BCM94343WWCD1_EVB Evaluation

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Working with WICED-Studio-5.2, Win7, BCM94343WWCD1_EVB Evaluation

WICED Evaluation boards have a FTDI FT2232 chip which provides debug capability with USB to UART+JTAG.Sample source can download to the Board and run,add the build target to ‘snip.uart-BCM94343WWCD1-debug download’, but debugging of the snip.uart sample app on the BCM94343WWCD1_EVB   always fails.

when Debugging failed even if you push F8,It will not respond to anything,Stop debugging and it will move properly。

screenshot As shown below

last_built.PNG

Sometimes when Debugging success 、As shown below

正常debug.PNG

How can solve the problem?

0 Likes
1 Solution
1 Reply