Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

NiMc_1688136
Level 5
Level 5
10 sign-ins 50 questions asked 10 solutions authored

I am trying to run the snip\ping_deepsleep example with FreeRTOS and LWIP. The application is crashing (hitting assert) right after getting the DHCP address.

In LwIP, pbuf.c, pbuf_free function, the application stops at LWIP_ASSERT("pbuf_free: p->ref > 0", p->ref > 0) where p->ref == 0.

The issue occurs in SDK 6.1 (lwIP 2.0.2) and 6.2 (lwIP 2.0.3).

Device: CYW43907

Console out

Application started: cur_rtos_time=0 cur_slow_time=92403407 rtos_time_since_deep_sleep_enter=2800103 wakeup_count=1

Cold boot.

Initialising LwIP v2.0.2

DHCP CLIENT hostname WICED IP

WLAN MAC Address : B8:D7:AF:28:B6:72

WLAN Firmware    : wl0: Feb 12 2018 23:35:27 version 7.15.168.108 (r683813) FWID 01-81fd72af

WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-02-12 23:30:46

WICED inited: rtos_time_since_deep_sleep_enter=2800787

Networking is about to bring up

Setting IPv6 link-local address

Obtaining IPv4 address via DHCP

IPv6 Network ready IP: FE80::BAD7:AFFF:FE28:B672

IPv4 Network ready IP: 192.168.1.100

Call tree (using lwip v2.0.2)

tcpip_thread, msg->msg.inp.input_fn(msg->msg.inp.p, msg->msg.inp.netif);     ( line 134)

    ethernet_input, etharp_input(p, netif);    (line 199)

         etharp_input,  pbuf_free(p);     (line 739)

I tried the same example with ThreadX and NetX Duo (my application needs FreeRTOS btw). If i run the application I get the stats message repeating:

stats: up_num=94 up_time=13165 max_up_time=0 wait_up_time=696 cpu_timer(cold=115601560 warm=0) pmu_timer(cold=112578747 warm=0)

wiced_network_save_dhcp_state_for_deep_sleep

If i debug the application then I hit an assert statement in wiced_network_resume_layers: wiced_assert("WICED can't resume DHCP client", 0 != 0 );

I have verified that pings do not work through wireshark monitoring and monitoring current consumption on a scope.

6 Replies
NiMc_1688136
Level 5
Level 5
10 sign-ins 50 questions asked 10 solutions authored

I am still not able to ping with this demo app

build string: testProjects.ping_deepsleep-CYW943907AEVAL1F-FreeRTOS-LwIP download run

I change platforms to the CYW943907AEVAL1F.

I am not getting the assert error in LwIP but I am getting the stats printout over and over, about 10s intervals.

Starting WICED vWiced_006.002.000.0072

Platform CYW943907AEVAL1F initialised

Started FreeRTOS v10.0.1

Initialising LwIP v2.0.3

DHCP CLIENT hostname WICED IP

WLAN MAC Address : A4:08:EA:D9:BA:8A

WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905

WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15

WICED inited: rtos_time_since_deep_sleep_enter=534948

Networking is about to bring up

Joining : AWS_Test_Network_24

Successfully joined : AWS_Test_Network_24

Setting IPv6 link-local address

IPv6 Network ready IP: FE80::A608:EAFF:FED9:BA8A

IPv4 Network ready IP: 192.168.1.59

Networking inited

CONSOLE: 1 wl0: wl_open

CONSOLE: 000002.632 wl0: link up (wl0)

stats: up_num=10 up_time=7153 max_up_time=0 wait_up_time=36 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=16 up_time=7862 max_up_time=0 wait_up_time=76 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=23 up_time=8278 max_up_time=0 wait_up_time=132 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=27 up_time=8354 max_up_time=0 wait_up_time=171 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=32 up_time=8729 max_up_time=0 wait_up_time=213 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=37 up_time=8799 max_up_time=0 wait_up_time=256 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=42 up_time=8869 max_up_time=0 wait_up_time=299 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=47 up_time=9233 max_up_time=0 wait_up_time=338 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=52 up_time=9302 max_up_time=0 wait_up_time=380 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=56 up_time=9353 max_up_time=0 wait_up_time=410 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=61 up_time=9727 max_up_time=0 wait_up_time=452 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=67 up_time=9814 max_up_time=0 wait_up_time=500 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=72 up_time=9883 max_up_time=0 wait_up_time=542 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=76 up_time=9938 max_up_time=0 wait_up_time=576 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

stats: up_num=81 up_time=10298 max_up_time=0 wait_up_time=615 cpu_timer(cold=144633789 warm=0) pmu_timer(cold=17647580 warm=0)

0 Likes

Appears the application is never entering the deepsleep mode.

wakeup_count is always set to 1 since the module does not reset from a deep sleep timeout.

wakeup_count needs to increment in order to trigger a ping.

I built the project with the original SDK 6.2 codebase  with FreeRTOS & LwIP and on the second boot, the project crashes with what seems to be a IDLE task stack overflow (if running in debug). The current does not appear to drop during the 10s supposedly in deep sleep.

Starting WICED vWiced_006.002.000.0072

Platform CYW943907AEVAL1F initialised

Started FreeRTOS v9.0.0

Initialising LwIP v2.0.3

DHCP CLIENT hostname WICED IP

WLAN MAC Address : A4:08:EA:D9:BA:8A

WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905

WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15

WICED inited: rtos_time_since_deep_sleep_enter=5075895

Networking is about to bring up

Joining : AWS_Test_Network_24

Successfully joined : AWS_Test_Network_24

Setting IPv6 link-local address

Obtaining IPv4 address via DHCP

IPv6 Network ready IP: FE80::A608:EAFF:FED9:BA8A

IPv4 Network ready IP: 192.168.1.104

Application started: cur_rtos_time=0 cur_slow_time=1739 rtos_time_since_deep_sleep_enter=52 wakeup_count=1

Cold boot.

Starting WICED vWiced_006.002.000.0072

Platform CYW943907AEVAL1F initialised

=== EXCEPTION ===

Debug event (e.g. breakpoint)

DFSR : 0x00000000

DFAR : 0x00000000

IFSR : 0x00000002

IFAR : 0x004B621C

CPSR : 0x00000197

R0   : 0x00000001

R1   : 0x00000000

R2   : 0x00000080

R3   : 0x00000001

R4   : 0x04040404

R5   : 0x05050505

R6   : 0x06060606

R7   : 0x00512370

R8   : 0x08080808

R9   : 0x09090909

R10  : 0x10101010

R11  : 0x11111111

R12  : 0x6573696C

LR   : 0x004B621C

=================

PriyaM_16
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

Hello,

There are some issues in ping_deepsleep app in WICED 6.2. We are looking into the issue. I will update the thread when the fix is available

Hello,

I'm experiencing what I think to be a very similar issue, if not the same issue, with the CYW943907AEVAL1F board and the ping_deepsleep snip app.

The board seems to be resetting over and over. Here is an extract of the console log:

Cold boot.

Starting WICED vWiced_006.002.001.0002

Platform CYW943907AEVAL1F initialised

Started ThreadX v5.8

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : 44:91:60:28:58:AE

WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905

WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15

WICED inited: rtos_time_since_deep_sleep_enter=218

Networking is about to bring up

Joining : PARADIGMA_2.4

Successfully joined : PARADIGMA_2.4

Obtaining IPv4 address via DHCP

DHCP CLIENT hostname WICED IP

Unable to restore dhcp state

IPv4 network ready IP: 172.16.94.171

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:4691:60FF:FE28:58AE

Networking inited

CONSOLE: 2 wl0: wl_open

CONSOLE: 000003.652 wl0: link up (wl0)

CONSOLE: 000003.658 wl0.0: wlc_send_bar: seq 0x1 tid 0

stats: up_num=30 up_time=14394 max_up_time=0 wait_up_time=141 cpu_timer(cold=9529250 warm=0) pmu_timer(cold=1472 warm=0)

wiced_network_save_dhcp_state_for_deep_sleep

Application started: cur_rtos_time=0 cur_slow_time=1472 rtos_time_since_deep_sleep_enter=44 wakeup_count=1

Cold boot.

Starting WICED vWiced_006.002.001.0002

Platform CYW943907AEVAL1F initialised

Started ThreadX v5.8

Initialising NetX_Duo v5.10_sp3

Creating Packet pools

WLAN MAC Address : 44:91:60:28:58:AE

WLAN Firmware    : wl0: May 15 2018 19:39:17 version 7.15.168.114 (r689934) FWID 01-d6f88905

WLAN CLM         : API: 12.2 Data: 9.10.74 Compiler: 1.31.3 ClmImport: 1.36.3 Creation: 2018-05-15 19:33:15

WICED inited: rtos_time_since_deep_sleep_enter=218

Networking is about to bring up

Joining : PARADIGMA_2.4

Successfully joined : PARADIGMA_2.4

Obtaining IPv4 address via DHCP

DHCP CLIENT hostname WICED IP

Unable to restore dhcp state

IPv4 network ready IP: 172.16.94.171

Setting IPv6 link-local address

IPv6 network ready IP: FE80:0000:0000:0000:4691:60FF:FE28:58AE

Networking inited

CONSOLE: 2 wl0: wl_open

CONSOLE: 000003.708 wl0: link up (wl0)

CONSOLE: 000003.713 wl0.0: wlc_send_bar: seq 0x1 tid 0

stats: up_num=34 up_time=16310 max_up_time=0 wait_up_time=167 cpu_timer(cold=9528623 warm=0) pmu_timer(cold=1472 warm=0)

wiced_network_save_dhcp_state_for_deep_sleep

Application started: cur_rtos_time=0 cur_slow_time=1472 rtos_time_since_deep_sleep_enter=44 wakeup_count=1

And this sequence keeps repeating over and over. The current never drops to be even near what it would be expected from a deep sleep state.

Is there a way to use deepsleep functionality with this hardware? The issue was reported 7 months ago and this thread has never been updated since then.

0 Likes

PriyaM_16 wrote:

Hello,

There are some issues in ping_deepsleep app in WICED 6.2. We are looking into the issue. I will update the thread when the fix is available

It has been quite long time since you replied. So any update? Is this still an issue?

0 Likes