Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

Sort by:
jeco
Wi-Fi Combo
Hello, I opened an old program to update my electronic card by reinstalling WICED Studio 6.6.1. When attempting to program my card with JTAG , I recei... Show More
mlodhia
Wi-Fi Combo
We have been using WICED SDK for our FW application running on STM32 sensor hardware.We use WICED to connect to WiFi AP. Application uses HTTPS to con... Show More
SeFe_4295646
Wi-Fi Combo
Greetings,We're having an issue connecting to SOME of our prototype hardware via Seger JLINK  SWD mode.  It works fine on some boards but not others. ... Show More
Ostrovsky
Wi-Fi Combo
when I read the register of CHIPCOMMON_SR_CONTROL1 to check if the firmware initialized sr engine, it failed, so I wondered how to enable or disable t... Show More
Chih-YuanC_26
Wi-Fi Combo
Infineon AIROC Wi-Fi/Bluetooth Combo STM32 Expansion Pack is an extension of the CMSIS-Pack standard established by Arm. The pack is compliant with th... Show More
mineronarrow
Wi-Fi Combo
Hi Customer is developing with Murata 1GC on WICED.  They are sending with ux_device_class_cdc_acm_write. It is blocking.  It will stuck if other side... Show More
MaFa_974161
Wi-Fi Combo
Hello. I have the sequent problem: I have developed a board with CYW943907 and an FPGA. I have to store FPGA configuration file (1.5Mbyte of size) in ... Show More
AntonSadkov
Wi-Fi Combo
Good afternoon. I am facing HTTPS speed issue on CYW943907AEVAL1F platform. When downloading a file via HTTPS, the speed drops almost 8 times, relativ... Show More
MaFa_974161
Wi-Fi Combo
Hello. In a previous post I read that I can use TopJTAG Flash Programmer to drive ARM-USB-TINY-H From Olimex, so I've bought ARM-USB-TINY-H and I've d... Show More
Chrisn
Wi-Fi Combo
We have a platform that uses WICED Version 3.7.0-7. AN STM32F469 processor uses the WiFi/BT module LBEE5KL1DX. We're able to bond with and connect and... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.