Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

ClLe_4298871
Wi-Fi Combo
Hello,We are able to build a demo project in the WICED SDK (snip.bluetooth.ble_hello_sensor) and flash it onto our eval board, CYW94343WWCD1. We are t... Show More
Anonymous
Wi-Fi Combo
I am trying to implement a USB 2.0 host for a custom class on a CYW54907 wireless SoC (CYW943907AEVAL1F dev board). I would like to connect the host t... Show More
DaRa_4056336
Wi-Fi Combo
Hi,Currently using Neb1DX and I am trying to update BT UART speed from 115200 to 3000000 . After some searching and reading I found the function bt_ho... Show More
jina_4171326
Wi-Fi Combo
respected sir/mamnow, i'm using CYW54907 and initialize WiFi Access-point in this board. and i'm able to analysis WiFi beacon frame in wire-shark soft... Show More
HaE_4338486
Wi-Fi Combo
Hi,    Can anyone give me the clear picture of Collaborative Coex between Wifi & BT? Does it mean both can operate simultaneously without interference... Show More
HaE_4338486
Wi-Fi Combo
Hi,
solved msg Solved
In CYW4343W (Wifi+BT combo), is there any chance of interference among wifi & BLE? Is coexistence implemented in the H/W?If so how to enable it? Show More
jalic_4332871
Wi-Fi Combo
I am using two bcm 43438A, the two devices are putted into a shield box, then I  tested them in wifi mfg mode. One device sends 1000 package, the othe... Show More
MoNo_2793136
Wi-Fi Combo
I am using the Murata reference board which is based on the 4343W. Currently, I measured the effective TCP throughput at 4.3 Mega Bits/second. My test... Show More
BaGo_4138971
Wi-Fi Combo
Hi All,I tried to debug wiced source code (SDKv6.1), some time it works but some time it won't.  When it stop working i need to delete metadata folder... Show More
SiCu_4257751
Wi-Fi Combo
Context Based on the datasheet, both VBAT and VDDIO have a working range comprehensive of the value 3.3V (VBAT IS 3V-4.2V and VDDIO is 1.8V-3.3V).Ques... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.