Wi-Fi Combo Forum Discussions
text.format{('custom.tabs.no.results')}
Is 802.11v currently supported? If yes, could you please clarify how the WNM Sleep Mode can be used?
Hi,
Attached is a patch for WICED v3.1.2 that creates a new platform BCM943362WCD4_ext. The platform is very similar to the WICED platform BCM943362WCD4. In fact its the same hardware. However this platform creates a read only filesystem and put the WIFI firmware (along with any other resources ) in to this file system, the file system can then downloaded in to the external flash using the normal multi application targets. For example, use the make target
snip.scan-BCM943362WCD4_ext download download_apps
to create and test the scan application.
PS: a preliminary untested version was released before, however this one is tested and belief to be working.
Regards,
Bassem
Show LessWhen the Enterprise supplicant fails to connect (e.g., by employing settings on the radius server that prevent authentication of the WICED device), then I am calling the following function in order to reset things and "start again":
besl_supplicant_stop(&supplicant_workspace)
However, calling the function hangs because it waits indefinitely for the thread to exit when calling:
host_rtos_join_thread( &host_workspace->thread )
This function behaves normally if the WICED client is authenticated and connected to the access point. For example, if the access point goes down, then up, then I need to call besl_supplicant_stop and besl_supplicant_deinit in order to recover the link. This works Ok.
Any ideas?
Show LessI've been combing through the code and documents trying to figure out if the following added to the make file will enable the AES encryption of data that is written to, and read from, the SPI flash:
PLATFORM_SECUREDCT_ENABLED := 1
PLATFORM_SECURESFLASH_ENABLED := 1
GLOBAL_DEFINES += SECURE_SFLASH
I see many useful functions in the file spi_flash_compatible.c, but it is not clear to me if the above automatically enables these functions, or if they need to be manually employed when an SPI with hardware encryption features is connected.
Any guidance would be appreciated.
Thanks!
Show LessHi,
I am using CYW943907AEVAL1F development board. I am using GPIO buttons 1 and 2 in interrupt mode. I am facing an issue that when I press the button, the registered handler is not called and the application gets crashed. However, the polling mode is wotking fine, so there is no problem with the hardware I guess. Can you please let me know what I am missing?
Below is my application code. Whenever I press Button 2, the application crashes.
Show Less
#include "wiced.h"
wiced_semaphore_t semaphore;
void _SwitchHandler(void* arg) {
if (wiced_rtos_set_semaphore(&semaphore) != WICED_SUCCESS) {
return;
}
}
void application_start( )
{
/* Initialise the WICED device */
wiced_init();
if (wiced_rtos_init_semaphore(&semaphore) != WICED_SUCCESS)
{
return;
}
wiced_gpio_init(WICED_BUTTON2, INPUT_PULL_UP);
if (WICED_SUCCESS != wiced_gpio_input_irq_enable(WICED_BUTTON2, IRQ_TRIGGER_RISING_EDGE,
_SwitchHandler, NULL)) {
WPRINT_APP_INFO(("Failed to register handler\n"));
return;
}
while (wiced_rtos_get_semaphore(semaphore, 100) != WICED_SUCCESS) {
wiced_rtos_delay_milliseconds(100);
}
WPRINT_APP_INFO(("Button pressed.\n"));
}
Hello,
in order to speed up the downloading process time on the CYW943907AEVAL1F board, is there any way to download code and data directly to the RAM ?
Thank you.
Show LessHi,
In WICED code (43xxx_Wi-Fi) lwip version is 2.0.3.
Here lwip 2.0.3 is modified to support wi-fi drivers.
Is there any document that explains what changes are done in lwip to support wi-fi drivers ?
Show LessHi, I tried to install WICED studio version 6.4.0 on windows from here WICED-Studio 6.4.0 Installer (Windows) i did everything as described in README.txt file but after chosing directory where i want to install IDE occure error like this:
While i got around 200 GB free space on each partition of disc.
I am using windows 10 education and my java version is 8.
let me know if any information about my system or computer can help you solve this problem.
Thanks, Wojciech
Show LessI have implemented a form of OTA and write an image of our WICED binary (new firmware)
to the staging area. We then update the DCT so that it will upgrade on the next boot. So
far everything works fine.
However, I am seeing a problem if I inject a reset after the bootloader has started but
before the file has been completely updated. What I am seeing is that the board
fails to reboot.
Is this a known problem? Do you have any suggestions as to how to debug this
(debugging the bootloader, it seems difficult).
Thanks
Show LessIs there support for cortex M33 in the new revision of WICED STUDIO?
If not, is it possible to add it? did the GCC compiler supports it in case we add Cortex M33 to the toolchain?
Show Less