Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

harelTur
Wi-Fi Combo
Hi   Where this define nned to be? I use laird - Sterling EWB (Cypress 4343 ..and STM32f411) I dont find where this define. Show More
jusadams
Wi-Fi Combo
I started poking around to see if I can get my build files packaged up so we can use them during manufacturing. It looks like the normal build command... Show More
hoainguyen265
Wi-Fi Combo
Hi guys, In our application, we connect to wifi AP and do stuffs. If we got some issues like request http error or disconnect with mqtt broker, we wil... Show More
Félix_T
Wi-Fi Combo
I just upgraded the version of Wiced we are using from 6.4 to 6.6.1.1. When the code tries to set wwd_wifi_fast_bss_transition_over_distribution_syste... Show More
mmch
Wi-Fi Combo
Hi, Is there a clear centralized exhaustive list (and history) of know vulnerabilities in the CYW4343W (or all chips) firmware ? Browsing https://github.com/Infineon/wifi-host-driver... Show More
jabu_4847606
Wi-Fi Combo
Measuring the 5.8g signal at the FCC test lab and only seeing 8 dbm, when the documents have 13 dbm as an average.  I retuned the antenna and still me... Show More
MaFa_974161
Wi-Fi Combo
Hello. We develop a board with the same processor in CYW943907AEVAL1F. We mount CYPRESS S25FL064LABNFI010 instead of MX25L6433FZNI as FLASH.   I modif... Show More
andyinsuffolk
Wi-Fi Combo
Hi there, I am looking for an app note or more importantly some WICED sample code which will allow me to,  firstly connect a generic BT headset/speake... Show More
KuWa_1758891
Wi-Fi Combo
Hi,  We have used CYW43455 for connection test, and we were unable to get IP address to run iperf even the AP can get the MAC address.  the following ... Show More
sanees
Wi-Fi Combo
mbedTLS
solved msg Solved
We have used Wiced SDK for Type 1LD development. Wiced doesn't supports LWM2M protocol. We are trying to port an open source LWM2M implementation like... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.