Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

Sort by:
chch_4469616
Wi-Fi Combo
We want to use CYW943907AEVAL1F to receive video data from the (SDIO/ Ethernet) interface and then transmit it with wifi, which requires the wifi tran... Show More
FuLu_4591171
Wi-Fi Combo
I am debuging cyw43438 using SDIO, when downloading wlan firmware to cyw43438, I always met the error response form CMD53. The response is 0x00002800,... Show More
AkKo_4458241
Wi-Fi Combo
Hello.If a WPS connection is executed using the following functions, it will stop with an error.Please tell me the cause and countermeasure.Function u... Show More
Leo_liu1
Wi-Fi Combo
Hi Sir,     目前在考虑MCU+CYW20706实现headset的方案,通过wiced20706 demo.audio.headset发现有两种模式:Apps processor 以及standalone mode。如果使用standalone mode,那么不需要外部mcu参与,207... Show More
HiIg_4537276
Wi-Fi Combo
HelloFunction processing in the functions of WicedPlease tell me the sleep function.What we want to realize is as follows.----------------------------... Show More
user_1743026
Wi-Fi Combo
HiI use cyw43364 with wiced.I want to use coex with third-party ble.I want to disable SECI Coex and to enable 3 wire Coex.below is array in wifi_nvram... Show More
Eric_wang
Wi-Fi Combo
Environment: Linux:4.15, AT91SAMA5D27 processor hostlog:# ifconfig wlan0 updhdsdio_clk_kso_enab> op:KSO_SET, ERROR: try_cnt:20001, rd_val:ff, ERR:ffff... Show More
HiIg_4537276
Wi-Fi Combo
HelloI'm having trouble with breakpoints not working as expected during debugging.Compile, start debugging, create breakpoint, start, do these in orde... Show More
AkKo_4458241
Wi-Fi Combo
Hello. I use the following function to get the credentials needed to connect to the router.. Is there a way to stop the processing of this function fr... Show More
WaLo_3890256
Wi-Fi Combo
Hello experts,We have created a project on WICED 43xx_Wi-Fi sdk for STM32F412 MCU+43438 wlan chip. We have downloaded the make target such as "snip.sc... Show More