Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

user_4676541
Wi-Fi Combo
I have a device that I'm testing against, which is broadcasting beacons at 1Mbps, and my application on CYW43907 is not receiving them. It's capturing... Show More
mpzimmers
Wi-Fi Combo
Hi all - I've been given the task of maintaining a very old application built upon WICED 2.4.1. I'd like to use the function wwd_wifi_abort_scan() to ... Show More
hoainguyen265
Wi-Fi Combo
Hi guys, in our project we use both cyw43907 and cyw54907 with the shared code. But we want to detect if current chip type is cyw43907 or cyw54907 to ... Show More
HMT
Wi-Fi Combo
Hi,I want to understand something  when I get 1025 - INVALID_JOIN_STATUS - what can I do to cause it to connect?? When I get 1006 - NOT_AUTHENTICATED-... Show More
HyKi_4229111
Wi-Fi Combo
I have an embedded platform of BLE and WiFi combo (CYW4343W) with ST32F4xx CPU. I need to perform some of Bluetooth test over the platform to go to Bl... Show More
maku_3939256
Wi-Fi Combo
Hi, We have a requirement to control BLE Tx Power in our application running in advertisement mode. We need your help in decreasing the BLE Tx Power o... Show More
MaFa_974161
Wi-Fi Combo
Hello. In a previous post I read that I can use TopJTAG Flash Programmer to drive ARM-USB-TINY-H From Olimex, so I've bought ARM-USB-TINY-H and I've d... Show More
Chrisn
Wi-Fi Combo
We have a platform that uses WICED Version 3.7.0-7. AN STM32F469 processor uses the WiFi/BT module LBEE5KL1DX. We're able to bond with and connect and... Show More
DaEg_3292701
Wi-Fi Combo
Regararding: WICED 6.1 won't install - continually asks to choose a different location​FWIW I can install it on macOS but it won't run. Very annoying.... Show More
sanmm_199922
Wi-Fi Combo
Environment and SDK information:WICED version: 6.4Wi-Fi Module: Murata Type1GC Wi-Fi connection(to wireless LAN AP) is lost immediately after 11 hours... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.