Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

SaSh_283021
Wi-Fi Combo
How to specify in Snip.scan that it should only scan 2.4 GHz channels?I am using CYW43907.Thanks and Regards,Sapan Shah Show More
KEKA_4568351
Wi-Fi Combo
It is a confirmation whether the verification process of the SSL certificate of HTTPS communication is performed, but in the following header file,Sin... Show More
LuKo_4670956
Wi-Fi Combo
I'm trying to test snip.wifi_mesh using the CYW943907AEVAL1F development board.  Initially the build failed because CYW943907AEVAL1F was not in VALID_... Show More
TB_2319586
Wi-Fi Combo
I need to use Segger J-Link with CYQ954907AEVAL1F, but I am quite concerned, because there looks to be a short-circuit between the JTAG header and the... Show More
NiMc_1688136
Wi-Fi Combo
I want to verify that the powersave application in deepsleep is working as intended. I am using the CYW943907AEVAL1F eval board with the powersave tes... Show More
CEMI_4636996
Wi-Fi Combo
Hello,I am using the NXP imx8mmini board with a CYW43455 cypress module with Android 9 and kernel version 4.14.98. However the adapter does not suppor... Show More
CoCo_1816446
Wi-Fi Combo
I am using CY8CKIT-062-WiFi-BT dev kit and WICED Studio 6.4 on Windows 10.BACKGROUND:For my project, I want ble_advertisement_flag_value = BTM_BLE_GEN... Show More
EvRe_4610981
Wi-Fi Combo
Hi, I'm trying to run a snip example.bluetooth.serial_get_service from Wiced 6.4(win). But its coing to reset after 5seconds.. and does not start.I ch... Show More
anJa_4692871
Wi-Fi Combo
Just wanting to point out that the current URL linked to download Wiced Studio is dead and not allowing downloads: https://community.cypress.com/community/wiced-wifi/wiced-wifi-documentation... Show More
Sophie_Wang
Wi-Fi Combo
Hi CY Friend,我装了WICED STUDIO 6.4.0.  安装之前把sdk和IDE该删的都删干净了。config.eml和installer.exe放在一个文件夹里。但是还是显示filters off。请问你知道这种情况怎么办吗?谢谢sophie Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.