Wi-Fi Combo Forum Discussions
The HTTPS server that is called by the snip.https_server application dies with repetitive client requests.
If you simply build the default application (SDK 6.4), then run it, you will see that the server permanently fails if you send closely-spaced client requests. You can do this by simply making a bookmark to the device URL (e.g., https://192.168.2.157/apps/https_server/https_server_top.html), then clicking on the link in quick succession (e.g., 2 to 5 times/sec). After a few seconds of clicking, the server dies (Firefox indicates no further pages are served).
Note that the function http_server_deferred_connect_callback() still appears to be called, but nothing happens after it is called.
Any help is appreciated.
Thanks!
Show LessThe following log is output and the program does not work
Please refer to the confirmation items and answer
・Log
************************************************** **
** ERROR: WLAN: could not download clm_blob file
** FATAL ERROR: system unusable, CLM blob file not found or corrupted.
************************************************** **
·Checklist
When updating with OTA, the "Current Application" area is rewritten, but the "File System Image" of "External Flash" is not rewritten (because of ReadOnly).
Therefore, if you update the software that rewrites [\43xxx_Wi-Fi\resources\firmware\4343W\4343WA1.bin]
I think that the error occurs because "File System Image" of "External Flash" is not rewritten and only "Current Application" is rewritten.
*Maybe there is an error in wwd_process_clm_data()
Is the understanding correct?
And is there a solution?
Show LessI am using murata 1LD main controller(STM32F412+CYW43438).We collect the data and stored to flash.we are planning to use 8Gb flash for data collection and OTA.Does murata 1LD support serial nand flash
Show LessHi all -- new to Wiced.
I am trying to do something simple -- I want to change the color scheme of the IDE to a dark mode. I know that eclipse supports it -- I can see the themes in the Eclipse marketspace. Problem is that when I try to install them the install always fails because some dependency is missing -- it doesn't really matter which theme it is - they all fail.
Any pointers?
Regards,
Matt
Show LessI am using the WICED-Studio-6.4 under Ubuntu 16.04 OS and the WLAN CYW943907AEVAL1F and CYW954907AEVAL1F kits
I can build the mfg_test image for the 2 Kits and get them to work reliably using the wl tool supplied by the WICED under the WIndows OS.
The WICED Studio offers only the wl executable file for Windows os and I am interested to know how I can build the equivalent of Windows wlxxx.exe file for the Linux OS ?
I am just curious to know if there is an easy way to build the wl executable for Linuz from the various make file.
Thank
Regards
JM Gayet
Application Engineer
Rohde & Schwarz Inc
Show LessHello,
I have two CYW943907EVAL1F boards. I need to stream audio through wifi. I'm naive with this development board and with WICED studio. I ran through the WICED WIFI 101 tutorials to get familiar with the board and the IDE. So not sure where to start for designing this project. I really appreciate if someone can please help me with this or even put me in the right direction for designing this project.
Thanks,
Santosh
Show LessHi, I run code(43xxx_Wi-Fi\otr_fr) on Sterling-EWB(Laird).
Is the OTA flash layout belong to internal flash?
My question is how to setup Internal(STM32F412 1MB)+External(2MB) flash layout for OTA? in DCT?
internal flash: bootloader / DCT / Current Application
External flash: FileSystem / APP0 / APP1
WICED version: 6.4
OS: ThreadX
Platform: GitHub - LairdCP/ewb_wiced_demo: Demo firmware for Laird Connectivity Sterling-EWB
Many thanks.
Billy C
Show LessI am wokring on Murata1LD board in Wiced-Studio.
Is there any structure or structure variable that gets updated based on the parameter passed to wiced_framework_set_boot() function.?
Came across a structure named "boot_detail_t. Is there any variable in this structure that gets updated based on DCT_APP0_INDEX, DCT_APP1_INDEX or DCT_APP2_INDEX that is passed to wiced_framework_set_boot() function?
Wiced_sdk: 6.4
OS: ThreadX
Please provide some information on this.
Thanks,
Binsy M S
Show LessI am using snip.config_mode as a starting point or my project and want to use a local wifi_config_dct.h file. I modified config_mode.mk to include the line
WIFI_CONFIG_DCT_H := wifi_config_dct.h
and everything builds as expected.
The problem occurs when I run it. When the default_wifi_config_dct.h is used the program works as expected, the web server is started and it acts as a soft ap, when the local copy is used, the program tries to join the the SSID defined by CLIENT_AP_SSID in the wifi_config_dct.h file.
The problem seems to occur in the function wiced_configure_device() when it calls wiced_dct_read_lock() getting the device_configured state. When default_wifi_config_dct.h is used, device_configured returns WICED_FALSE, when the local copy (an identical copy) is used WICED_TRUE is returned.
What am I missing? Is there a document I should be reading?
Thanks in advance
Show LessHello,
I am working on Murata1LD board in WicedStudio.
I want to place apps to DCT_APP0_INDEX and DCT_APP1_INDEX. I am able to write apps to both these locations. But changing boot sector using function wiced_framework_set_boot() and rebooting always boots with app present in DCT_APP0_INDEX. Do you have any documents explaining the boot loader flow? I am also looking for a way to identify from which partition the app is loaded.
WICED version - 6.4
OS - ThreadX
Please give some guidelines on this.
Thanks,
Binsy M S
Show Less