Wi-Fi Combo Forum Discussions
text.format{('custom.tabs.no.results')}
[WICED-SDK-2.2.1]
I cant connect with an AP using WPS when the security setting is WEP, WPA-AES or WPA2-TKIP.
Is this by design for WPS or is it a bug?
Show Less[WICED-SDK-2.2.1]
Im trying to do a UDP broadcast on port 56700, do I send it on an IP address of 255.255.255.255
should my wiced_udp_send call look like this?
const wiced_ip_address_t INITIALISER_IPV4_ADDRESS( target_ip_addr, 0xFFFFFFFF ); .
.
.
.
wiced_udp_send(&udp_socket, &target_ip_addr, 56700, packet)
Is there anything special I need to enable?
Show Less[WICED-SDK-2.2.1]
My application requires multiple TCP sockets to be open simultaneously. How many are supported in WICED? Is this dependent upon the RTOS?
Show LessJason,
Is it possible to have 3 UART on WICED? The API defined only 2 inside, does it mean that we only can support 2 UART interface?
For the hardware connection, I am confirming with USI engineer. This is the request from Haier. Haier plan to connect the NFC module to WICED by one more UART.
Show Less