Wi-Fi Combo

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
sanmm_199922
Wi-Fi Combo
Environment and SDK information:WICED version: 6.4Wi-Fi Module: Murata Type1GC Wi-Fi connection(to wireless LAN AP) is lost immediately after 11 hours... Show More
AxLi_1746341
Wi-Fi Combo
@PriyaM_16  In this thread:https://community.infineon.com/t5/Wi-Fi-Combo/usb-device-cdc-sample-can-not-send-512byte/m-p/240409The comment says it's a ... Show More
cblack-f3
Wi-Fi Combo
We are looking for some information on rough memory footprint data on simultaneous BLE/WLAN examples - using the ST+Cypress part (LBEE5PA1LD).  Some t... Show More
AxLi_1746341
Wi-Fi Combo
The WICED-6.6.1.1 is using mbedTLS-2.16.6, which includes some security issues:https://tls.mbed.org/security Please upgrade mbedTLS to the latest stab... Show More
skarphedinnos
Wi-Fi Combo
As far as is understand is that when wiced_rtos_get_semaphore is called, it decrements the semaphore counter until the counter is zero. If the counter... Show More
BeOl_4470266
Wi-Fi Combo
Hello, When could we expect support for the LwIP Chained Buffers? At the moment, Wiced does not properly support LwIP without this. The Chained Buffer... Show More
MaFa_974161
Wi-Fi Combo
Hello. I noticed this strange behaviour for USBX CDC ACM: it sometimes fails when "Write" less than 8 bytes. You can test this from "snip/usbx_usb_dev... Show More
AxLi_1746341
Wi-Fi Combo
The WICED-6.6.1.1 is using lwIP-2.0.3, which was released 4 years ago.So the WICED users may hit some issues that had been fixed by upstream lwIP. Cur... Show More
lili_4421586
Wi-Fi Combo
Hi,  we are developing software on CYW43907, power consumption is very critical for us. we put CYW43907 APP CPU into sleep mode when no data send,  an... Show More
RoMc_863046
Wi-Fi Combo
Hello,I am trying to configure SPI Slave on STM32F4xx in the Laird EWB Platform.  The Host MCU is STM32F412.I have added SPI4 on the STM32 to the Wice... Show More
Board Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.
Top liked authors