Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

Sort by:
BaRu_3629256
Wi-Fi Combo
I am looking into speeding up the time it takes for my device to connect to an AP. A network packet capture is showing a delay of about 2.2 seconds be... Show More
AntonSadkov
Wi-Fi Combo
Good afternoon. I am facing HTTPS speed issue on CYW943907AEVAL1F platform. When downloading a file via HTTPS, the speed drops almost 8 times, relativ... Show More
gzap
Wi-Fi Combo
Hi. I am trying to use mbedtls library with TLS 1.3 support in WICED studio. I am looking for the BESL supplicant library source code in order to chec... Show More
IVPB
Wi-Fi Combo
We are evaluating the Murata Type 1GC Wi-Fi chip using WICED SDK and 43xxx_Wi-Fi project provided.  ref: https://www.murata.com/-/media/webrenewal/products/connectivitymodule/asset/pub/rfm/data/n1-5002_type1gc_1ps-quick_start_guide.ashx?la=en&cvid=20211022010000000000... Show More
BaRu_3629256
Wi-Fi Combo
I am looking into speeding up the time it takes for my device to complete a 2-way TLS handshake. A network packet capture is showing that this process... Show More
dvir92
Wi-Fi Combo
Hiwe designed a custom board that contains the wifi module: EWB-STERLING,(453-00014R )In my board, I routing the USART1 pins to FTDI chip (FT4232 with... Show More
NiMc_1688136
Wi-Fi Combo
WICED SDK 6.6.1.1 WLAN Firmware : wl0: Mar 31 2022 01:31:05 version 7.15.168.156 (4f1e919) (pulled from Modus) I see references in the release notes a... Show More
user_4676541
Wi-Fi Combo
I have a device that I'm testing against, which is broadcasting beacons at 1Mbps, and my application on CYW43907 is not receiving them. It's capturing... Show More
mpzimmers
Wi-Fi Combo
Hi all - I've been given the task of maintaining a very old application built upon WICED 2.4.1. I'd like to use the function wwd_wifi_abort_scan() to ... Show More
hoainguyen265
Wi-Fi Combo
Hi guys, in our project we use both cyw43907 and cyw54907 with the shared code. But we want to detect if current chip type is cyw43907 or cyw54907 to ... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.