Wi-Fi Combo Forum Discussions
Hello,
This looks like a separate board for using with iOS? Can't the same WICED board be used with iOS? I am sure it must be using the same radio....any hardware differences??
Thanks,
-Gitesh Kulkarni
Show Less环境:WICED-SDK-2.3.1
问题:Apps工程下,编译wwd.appliance-BCM943362WCD4 download run,提示Apps/wwd/appliance/FreeRTOS_LwIP_appliance.c:52:22: fatal error: lwip/opt.h: No such file or directory,如图所示,我应该在哪个Makefile文件中,添加opt.h头文件的路径 ?请帮忙,谢谢!
Show LessI'm having an issue where I never get a scan complete event in my application containing critical sections (aka, scheduler and interrupts disabled). If I try running the example scan snippet, I see that a scan complete event occurs; however, in my application it does not. I have determined that this error occurs due to never receiving scan complete event from the 43362 chipset. I determined this by inspecting the status of every ASYNCEVENT_HEADER message in the event handler loop of 'wiced_process_sdpcm' in 'SDPCM.c' and logging any messages containing the correct status value.
Now, I'm running WICED 2.3.1, not 2.4.x. I understand that 2.4.x resolves some issue with SDIO Bus reliability. Is this the issue I'm seeing? Or is there something else that can trigger what I'm encountering?
-Dan
Show LessHello
When I was doing usart data sent to the TCP encountered a problem:
Somewhile ,when I through the usart send “abcdefg” to the BCM943362WCD4 , It can receive the data ”abc”. But it lost the data “defg”. And I send “abcdefg” to the BCM943362WCD4 again, It receive the data ”defgabcdefg”.Why is this?
My English is not good, I hope you can understand ^_^ thx.
Show Lesswhile(1){
while (wiced_uart_receive_bytes( WICED_UART_1, &c, 1, 1 )==WICED_SUCCESS )
{
rxbuf[rxcount++]=c;
readflag=true;
}
if(readflag==true)
{
wiced_tcp_send_buffer( &tcp_client_socket,rxbuf,rxcount);
wiced_uart_transmit_bytes( WICED_UART_1,rxbuf,rxcount);
memset(rxbuf,0,rxcount);
rxcount=0;
readflag=false;
}
}
Hello,
I have noted that SDK is compatible for SAM4 of Atmel.
If the Host Processor is going to be SAMA5D3X, what actions should be done in order to use WICED in Linux environment?
Thanks!
Eyal
Show LessHello All,
Is the WICED 4.2 WiFi OSx IDE installer package still available?
I try to download but get this error:
Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.
Bruce
Show LessAfter some time module (in AP mode) becomes unresponsive for a few seconds. After that it again starts processing requests.
For example:
Reply from 192.168.0.1: bytes=100 time=3ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=8ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=1ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=1ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=3ms TTL=128
Request timed out.
Request timed out.
Reply from 192.168.0.1: bytes=100 time=1725ms TTL=128
Reply from 192.168.0.1: bytes=100 time=3ms TTL=128
Reply from 192.168.0.1: bytes=100 time=3ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=10ms TTL=128
Reply from 192.168.0.1: bytes=100 time=12ms TTL=128
Reply from 192.168.0.1: bytes=100 time=1ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=3ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Reply from 192.168.0.1: bytes=100 time=1ms TTL=128
Reply from 192.168.0.1: bytes=100 time=4ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Request timed out.
Request timed out.
Reply from 192.168.0.1: bytes=100 time=1352ms TTL=128
Reply from 192.168.0.1: bytes=100 time=11ms TTL=128
Reply from 192.168.0.1: bytes=100 time=2ms TTL=128
Does anyone have a clue what is going on? Thank you and kind regards, Matej
Show Less