Wi-Fi Combo Forum Discussions
Just doing "iperf --help" makes the iperf app throw a hardware exception. I have modified the iperf.mk to have less buffers. the particular STM processor I use has 756K Flash and 96K Ram. iperf that is on WICED-SDK-2.2.1 works on the same hardware. Is there anything changed from SDK2.2.1 to SDK2.3.1 related to the iperf app? Does anyone have the similar issue???
Show LessHi,
I am using BCM943362WCD4 WICED-Wifi Eval board. I want to try the Easy Setup using Cooee example in WICED SDK-2.4.0. But I am using Linux OS. Is the Cooee client (easy_setup_cooee.exe for Windows) available for Linux ?
If not, will it be available in SDK-3.0.0 ?
Another question, Where can I download SDK-3.0.0 for BCM943362WCD4 ? Does it has enhanced features than SDK-2.4.0 for my Eval board ?
Show LessHi,
I'm curious about this malloc_transfer_to_curr_thread because it's an empty define. All malloc is allocated from the global pool (in ThreadX) so i suppose from people who are using ThreadX there is no need for such transfer am i correct? But why is there such define and also used across some WICED App project if the implementation is empty??
Show LessIn the dct.c, I had to change the line 20 from
#include "wifi_config_dct.h"
to
#include WICED_WIFI_CONFIG_DCT_H
To allow WIFI_CONFIG_DCT_H in the makefile. Am i missing something?
Show LessUsing a client with wiced_tls_init_simple_context() we cannot get an encrypted connection to receive data. The client disconnect after we send data over the connection.
Is there any more documentation available how to set up a tls tcp connection to a server? Or methods to debug other then tpc_error?
regards,
Jasper
Show LessDear Sir,
I have a question for the sequence of scan.
When I try to scan AP, the name of AP listed is different every time at the same location.
1. Is it possible to list them up for name order or RSSI?
2. Is there any option to decide the sequence of the list?
3. Could you let me know how can the list sequence be decided ?
Please, review below and let me know the way if there is.
Thank you in advance.
1st Scan
00:12:17:71:36:9C -73 cel#202
00:08:9F:16:38:ED -40 celizion#sw3
04:9F:06:90:A9:FD -60 INSU.KIM
00:40:5A:B3:4C:18 -82
00:12:47:F3:62:47 -73 powergps
00:15:70:C4:C5:90 -90 kpic0810
00:23:AA:12:02:66 -55 HW_TEST_2G
80:1F:02:C6:11:E0 -82 1042016
00:08:9F:B1:8D:18 -78 Chunma ENG(Civil)
00:26:66:B5:1D:4C -72 Beijing
00:14:CD:30:45:FF -75 WeVO_AP
00:1F:1F:16:F7:38 -69 anygate
64:E5:99:2E:65:C2 -78 sn
00:26:66:86:38:5C -82 iloveasset(HQ)
00:26:66:21:20:6C -85 chunma
08:10:76:98:C7:1A -61 netis 2G
2nd Scan
00:12:17:71:36:9C -80 cel#202
00:08:9F:16:38:ED -57 celizion#sw3
04:9F:06:90:A9:FD -62 INSU.KIM
00:12:47:F3:62:47 -72 powergps
00:15:70:C4:C5:90 -86 kpic0810
80:1F:02:C6:11:E0 -84 1042016
00:23:AA:12:02:66 -53 HW_TEST_2G
00:08:9F:79:A0:70 -80 daroom
00:26:66:31:B4:A0 -79 iptime
00:08:9F:B1:8D:18 -81 Chunma ENG(Civil)
00:40:5A:C8:B6:E0 -83
00:26:66:B5:1D:4C -75 Beijing
00:14:CD:30:45:FF -77 WeVO_AP
64:E5:99:2E:65:C2 -84 sn
00:1F:1F:16:F7:38 -74 anygate
08:10:76:98:C7:1A -60 netis 2G
Show LessHI,
How can I detect a socket disconnection?
I have a socket connected to a machine somewhere, if the remote machine closes the socket, how can I detect that event?
I tried:
wiced_tcp_register_callbacks
But the callbacks are never called. Is there a way to say something like:
If(SocketIsConnected(socket)) {
//do something
}
Thanks
Show LessHave any of you people changed the firmware to your own in the Murata SN8200 device?
I got a little further by using the BCM943362WCD2 target in the current SDK
My hope was the use the SN8200 with updated firmware (similar to their SNIC API) to host a mini server and my own application on the module itself.
Show Less