Wi-Fi Combo Forum Discussions
Hi
Any app I try to debug with Eclipse fails when calling wiced_bus_init.
The same app works perfectly when just downloading it and running it.
Only a few times out of hundreds of tries it worked with the debugger.
I use the Broadcom BCM943362WCD4 evaluation board.
Any ideas how to solve this?
Thanks
Show LessWhat is the appropiate way to configure the speed of the serial port dinamically? In the application the serial port needs to be reconfigure every time that establish the communication with the Host MCU, since the communication started at certain speed and after needs to be changed. We tried open and close the serial port on the STM3 MCU but the system stop operating correctly, no more information sent.
they only way to make it work, was overwritting the configuration of the port. Is this the correct procedure?
Gerardo
Show LessIs the STM32L series a good option to pair with the BCM43341? I care about ultra low power consumption for an extremely low duty cycle application (leakage power can potentially dominate). STM32F is nice but not great at ULP, although it offers SDIO and hardware based encryption for SSL/TLS stuff. I'd like to know about potential scenarios with other families as well (EFMs, MSP430 etc).
Thanks.
Show LessIs possible to change the power gain of the amplifier? I have a customer that is experiencing connectivity issues after they insert their PCB into their box, plastic based.
thanks,
Gerardo @ Insight
Show LessHi,
I was wondering if anybody has been able to connect to a server using TLS 1.1? It says in WICED WiFi FAQ (WICED Wi-Fi FAQ) that the SDK supports up to TLS 1.1 but I have been unable to connect using TLS 1.1. I have been able to connect to it using TLS 1.0. The server I am trying to connect to supports TLS 1.0 and TLS 1.1.
Thanks in advance.
Genu
Show LessI've noticed a change in behaviour when calling 'wiced_wifi_get_associated_client_list()'. In WICED 2.3.1 the call returned a list of the clients currently associated with the Soft AP interface (as expected.) In WICED 2.4.0 the list now includes an entry for the AP with which the STA interface is associated. Is this an intentional change?
Show LessWe are working with WICED 2.4.1 and have some questions about accessing functions in the 43362 chip
1. How do we configure the Bluetooth coexistence GPIO’s 3, 4, and 5 as inputs?
2. How do we configure the GPIO’s with a pullup or pulldown?
3. How do we read the states of the gpio inputs?
this is apparently all done via the SDIO bus, using wiced api calls.
Thanks.
Show LessHello,
I'm looking into how best to setup a secure webserver with WICED and I found the sample certificates that are provided with the SDK (Resources/certificates/). Given that this appears to be a valid certificate for a broadcom subdomain purchased from Entrust.net, is there not a concern that someone could use this certificate to host a real website at 'securedemo.wiced.broadcom.com'?
I don't have any nefarious plans myself, but this would be the concern I'd have (perhaps unnecessarily?) with purchasing our own certificate from a CA for 'mydevice.mydomain.com' and programming it into every device we manufacturer. If an attacker managed to extract the certificate data from our hardware, would he then not be able to host a site on the broader internet at 'mydevice.mydomain.com' and trick various DNS servers to direct people there who would then think it's a trustable 'mydomain.com' website?
Perhaps DNS spoofing is a thing of the past(?) I'd certainly like to take the above approach because it prevents users from being prompted with an 'untrusted certificate' warning when accessing the secure WICED webserver, but I can't risk any security vulnerabilities.
Thanks!
Show Less